f. m. said: You don't have/use a link library build for ARM code instead of Thumb2, do you ?
I'm not sure if I understand your question. I didn't use a precompiled library. I'm not very deep into the different instruction sets and because of the missing…
Connected it through Debug to the accompanying USB cable into laptop's USB port. Moved the switch to Debug setting. The lights go on as expected, with one light changing. The buttons work as expected too. However, my computer is not recognizing the Launchpad…
I am using Labview and LM4F120XL through serial communication. But it seems using basic_serial_write_read.vi cannot change the baud rate other than 9600bps. I am sure the code in LM4 is right because I use it through putty. But I don't know why VISA.vi…
I ordered two Stellaris Launchpad one of them works correctly and without any problem.
The second one however it is not recognized by the PC, it always shows one "In-Circuit Debug Interface" in device manager.
I have tried different USB ports and…
Other Parts Discussed in Thread: TM4C123GH6PM Greetings:
I am moving some code from an LM4F120XL launchpad to the TM4C123GXL launchpad and moving from Stellaris to Tiva. This code worked on the 120 but I have not been successful in getting it to run…
Hello,
I tried testing the codes from C:\ti\TivaWare_C_Series-2.0.1.11577\examples\boards\ dk-tm4c123g \boot_demo1 on
Stellaris LAUNCHPAD (LM4F120XL) . I used LM Flash Programmer to build the Boot Loader Program and in next step configured it to Manual…
hello guys,
I am using Stellaris EKLM4F120XL evaluation kit which is almost equal to Tiva board.At first I used to run any code and it used debug successfully with IAR Embedded workbench .After I ran qs-rgb programme given in stellarisware .It also…
Hello,
My fellow colleague was messing around with the Stellaris and accidentally left the LM4F120 Launchpad in sleep mode. The current draw is that of 9mA which is the average we were getting when it was entering sleep mode. We've been reading of solutions…