Part Number: ESD122 I am looking for a device to provide USB2.0 protection, and powered by 3.3V. Does the ESD122 provide back drive protection? If not, can you recommend a device that does? Thank You.
Back to Interface Home Page
USB Protection
Highlights:
USB Type-CTM has a 24-pin connector that can support USB 3 .1 Gen2, DisplayPort, HDMI, and a variety of other alternate modes:
SuperSpeed USB lines for USB 3 .1 Gen2 (Tx1+, Tx1–, Rx1+, Rx1–, Tx2…
Part Number: ESD122 Other Parts Discussed in Thread: TPD2E2U06 , TPD1E01B04 , TPD1E1B04 , TPD1E04U04 Hi Sir,
This table shows the comparison of ESD122 and RClamp3391ZC, which is used by the customer for USB2.0.
Do you think ESD122 is a suitable alternative…
Part Number: ESD122 Hi,
My customer is having problem of connecting the GND pin to the GND plane.
Below is the connection in the datasheet:
This is the way customer connect in the simulation, but the result is bad, can you help to suggest how can we…
Part Number: ESD122 Hi,
I intend to use the ESD122 to protect some PCIe 3.0 lines that go to a removable SSD. Is there any reason I can't use it for my 10G Ethernet lines also? It looks like a good fit but as Ethernet isn't listed in the applications…
Part Number: ESD122 Hi,
I would like to know more about the leakage of the ESD122.
First, it looks like the typical leakage is much lower, around 0.6 nA worst case on on Figure 8. Where does the 10nA of leakage situation come from?
Also, is there a worst…
Other Parts Discussed in Thread: ESD2CANXL24-Q1 , ESD2CAN24-Q1 , ESD2CANFD24-Q1 , ESD122 What should be considered when selecting a diode with parasitic capacitance?
Part Number: ESD122 Other Parts Discussed in Thread: ESD401 , HI Sir
I saw ESD401's Rdyn value is 0.7ohm smaller than ESD122's 0.5ohm
But ESD401's Air Cap and contact discharge value is better than ESD122
May I know the detail ?
As I know low…