Part Number: TUSB320LAI Other Parts Discussed in Thread: TMUXHS4212 , TPS25821 , TUSB321AI , ESD441 Tool/software: Hi Team,
Customer wants to replace an USB OTG interface with USB-C DRP (USB3.2 up to 1.5A) and use the TUSB320LAI for this use case…
Hi Vishesh,
Thanks . Maybe both implementations is great idea.
Can I raise another related question as below
When I use the TUSB320LI/TUSB320HT as a DRP controller with the Type-C port configured as a sink, sourcing up to 5V/3A from an external…
Part Number: TPD12S016 Other Parts Discussed in Thread: AM62P , AM625 , , ESD204 , ESD441 Tool/software: Hello Everyone,
We are interfacing HDMI with a microprocessor such as AM625 or AM62P for use in Industrial HMI Controller environment.
We would…
Hi Imelda,
Since the clamping voltage of this device is much higher than 5V, this device would not be effective with protecting the lower voltage VBUS. To protect a 5V USB VBUS line, I would recommend using ESD441 . There are a few different options…
Back to Interface Home Page
USB Protection
Highlights:
USB Type-CTM has a 24-pin connector that can support USB 3 .1 Gen2, DisplayPort, HDMI, and a variety of other alternate modes:
SuperSpeed USB lines for USB 3 .1 Gen2 (Tx1+, Tx1–, Rx1…
Below are the latest recommendations of devices for multiple interfaces that provide you IEC protection and paired with low capacitance that minimizes impact to bandwidth in the system. Please also refer to our System-Level ESD Guide for more details…
Other Parts Discussed in Thread: PSPICE-FOR-TI Back to FAQ Home Page
Interface Protection Guides
Part Recommendation
Packaging & Layout
Models
Transient Standards
System/Device Level Design
Power Dissipation…