Hi Brijesh :
Yes, I do run ./vision_app_init.sh before run_app_multi_cam.sh . And I did see the print from the mcu cores :
[MCU2_0] 5.500580 s: CIO: Init ... Done !!!
[MCU2_0] 5.500623 s: CPU is running FreeRTOS
[MCU2_0] 5.500635 s: APP: Init…
Hi Muniyappan, first we need to differentiate between frequency hopping for sleepy sensors and non sleepy sensors. You want to use sleepy sensors which means that all of these sensors follow the collector hopping and none of them follows an own sequence…
Yes, I ran this on a PC using edgeai-benchmark emulation. I’ve tested with the latest version, but the issue persists, and the accuracy remains 0.
Attached is my .yaml configuration file for reference.
common: target_module: 'vision' task_type: 'detection…
Part Number: EVM430-FR6043 Other Parts Discussed in Thread: MSP430FR6047 , MSP430FR6043 Tool/software: We are using EVM430-FR6043 with Ultrasonic sensor ( 500KHz ) for Air flow metering.
The airflow for 3-4 seconds is passed to do the waveform analysis…
Praveen, see images below. I took readings of Q3 gate, drain, and source triggered at the falling edge of Q2's gate. Gate and drain remain the same when Q2 gate drops because it's still charging, pushing the current back through Q3. The gate of Q3 oscillates…
I have added calibration process as per datasheet in my code. Now logs is as below BQ34Z100-G1 PbA demo starting...<CR><LF> Unsealed<CR><LF> PackCfg MSB=0x08 LSB=0x00 VOLTSEL(bit3)=0 TEMPS(bit2)=0 LED_COMM=0x93 NumSeries=12<CR><LF> REG(0x40) block0:<CR…
Hi Brijesh We made some more modifications and tested. 1. Discover by adding log: The GTC clock frequency value obtained through the Sciclient_pmGetModuleClkFreq() api in work/tda4/rtos-sdk/vision_apps/utils/console_io/src/app_log_rtos.c, Some cpu cores…
Hello Scott,
There are two non-P2P recommendations here TPS7A2015PDBVR which will meet the output current spec, however the IQ will be worse at roughly 6.5uA. The other alternative would be TPS7A0315PDBVR which will not meet the output current spec…