Hi Anuj,
I tried to dump isif. According to me in both the cases it is not working.
Here is the boot log when autorun.sh script is commented:
boot_log_moduletest_drv_isif.txt
Here is the boot log when autorun.sh is uncommented but boa is disabled…
Other Parts Discussed in Thread: CCSTUDIO I have been trying for the last week to install CCS 5.2 onto a new computer with no luck. It appears some of the features install but not all. I require assistance to the problem. Below is the log.
[ Edited…
Part Number: IWR1443BOOST I have installed the mmwave SDK version 1.2.0 and I am trying to obtain raw IQ samples. From this forum post and others I see that users were able to capture the raw ADC Buffer data using the capture demo. However, v.1.2.0 of…
Part Number: TMS320F28377S Other Parts Discussed in Thread: C2000WARE Hello, people!
Please, help me one more time.
I've read the document "F2837xS Peripheral Driver Library 2.00.00.02" in order to use the driverlib library properly, specially the…
Part Number: TPS6594-Q1 Other Parts Discussed in Thread: LP8764-Q1
This FAQ is relevant to TPS6594-Q1, LP8764-Q1, TPS6594x devices, and LP876x devices.
Yes! The Scalable PMICs devices are designed to be highly customizable, and as such customers…
Hi, attached are logs. First run is OK, during second run there is reset. It is also indicated in the log, that there was rtos-assert reset.
I tested also Linux SDK v. 2_08_00_04. The same behavior.
collector_log_firstRun.txt
collector_log_secondRun…
Hi,
In the settings application, when I move Bluetooth's toggle button from OFF to ON, it switches back to OFF right away. There is no serial output while toggling, but serial output on boot-up as well as LogCat output from both boot-up and toggling…
Would also recommend section 4.3 of this document. Describes the same HA application (albeit for a ZAP-ZNP operational model). This document is available from the MSP430-ZAP-1.0.3 installer from www.ti.com/z-stack
swrc173.zip (57.0MB) - contains ZStack…
Now i'm porting the IPNC3.1 release to our own board.But have some error .The following isthe boot info :
Please ti engineer to look at.
U-Boot 2010.12-rc2 (May 03 2013 - 17:45:15)
Cores: ARM 297 MHz DDR: 243 MHz I2C: ready DRAM: 128 MiB NAND: 256…
Part Number: AWR1443 Other Parts Discussed in Thread: UNIFLASH Hi
I am trying to capture demo by AWR1443
But it's my first time to use AWR1443 and CCS, so I failed at the first step.
In the guide mmwave_sdk_user_guide (1).pdf
Section 3. 4. 2.…