Part Number: EVMK2GX TI provides the PRU Ethernet firmware for K2G as follows: k2g-pru0-prueth-fw.elf k2g-pru1-prueth-fw.elf
K2G's Linux device tree (arch/arm/boot/dts/keystone-k2g.dtsi) has four PRU as follows: pru0_0: pru@20ab4000 pru0_1: pru@20ab8…
Part Number: 66AK2G12 Other Parts Discussed in Thread: EVMK2GX Hi,
The evaluation board "EVMK2GX" operates with evmk2g.gel which is installed with CCS.
(The GEL file location : C:\ti\ccs1010\ccs\ccs_base\emulation\boards\evmk2g\gel)
I cannot find…
Part Number: EVMK2GX Other Parts Discussed in Thread: SYSBIOS I installed CCS10.02 but I cannot find RTOS template application from C:\ti\processor_sdk_rtos_k2g_6_03_00_106\demos
Then I create simple rtos application by CCS project wizard.
Here is C code…
Part Number: EVMK2GX Hello,
I am looking to use the NAND flash connect on the GPMC on TI Eval Board 66AK2GG1, but I don t not see any point for NAND flash on /dev/mtd.
Started to look at device tree for keystone, I see there is no use of GPMC and/or…
Part Number: EVMK2GX Hello,
I am using K2G keystone, on eval board 66AK2GG1. Using TI Linux SDK 06_03_00_106, I am loading the kernel with arago-base-tisdk-image rootFS.
I would like to load DSP, but I notice there is no MPM (client nor Server) applications…
Part Number: EVMK2GX Other Parts Discussed in Thread: 66AK2G12 , CCS 10.2
pdk_k2g_1_0_16
processor_sdk_rtos_k2g_6_03_00_106
bios_6_76_03_01
Can you please fix the pdkProjectCreate scripts to create a CCS example project for DCAN? There is a zip file rtos_template_app_am572x_c66…
Part Number: EVMK2GX Other Parts Discussed in Thread: SYSBIOS "../framework/systemInit.c", line 276: error #20: identifier "TaskAfp" is undefined "../framework/systemInit.c", line 277: error #20: identifier "TaskAip" is undefined…
Part Number: EVMK2GX Hello,
On K2G EVM board, I inserted SD card, connect USB serial then I can capture below serial log, but system stuck here, no further load uboot, application, why?
BMC VERSION 0.6.1.0 BUILT Apr 11 2016 12:19:52 -------------------…
Part Number: EVMK2GX Hi,
I want to use Message manager for inter processor communication between ARM and DSP core. In ARM core i'm running Linux and on DSP core I want to run baremetal code. Is it possible to do it(as I am running baremetal on DSP) as…
Part Number: EVMK2GX Hi fellows,
the TRM of the 66AK2Gx states the following: "The Quad Serial Peripheral Interface (QSPI™) module is a kind of Serial Peripheral Interface (SPI) module which allows single, dual or quad read and write access to external…