Part Number: CC3135MOD Good Day,
1. I am using CC3135MOD interfaced with host MCU as STM32. As per the below mentioned thread in TI forum ( https://e2e.ti.com/support/wireless-connectivity/wifi/f/wi-fi-forum/995950/cc3135-latest-sdk?tisearch=e2e-sitesearch&keymatch…
Part Number: TMS320F2800137 Other Parts Discussed in Thread: C2000WARE While programming F2800137 using serial flash programmer utility, it works fine when we boot (SCI Boot Mode) the device using boot pins ( GPIO32 and GPIO24)
We are able to program both…
Hi Zoe,
thanks for your answer.
Now I can enable the CRC error flag. However, I am still not quite sure what the flag does if the CRC errors are already registered correctly without this flag. Is there a more detailed explanation of this? Do I understand…
Since uploading the file with the insert option isn't working for me and pasting the file directly crashes the page I'm splitting this into multiple sections of which this is the first.
#########################################################…
Part Number: SN65DSI83 We're using a sn65dsi83 chip to convert from 2-lane MIPI to LVDS.
The display panel wants a pixel clock in the range 66 to 70 MHz.
The DSI can only output at 83.33 (=500/6) or 62.5 (=500/8) MHz pixel clock, both are out of spec…
1. It is typo. Both eye test is on 0x4E 2. 0x4C device is setting as module to host. Both channel periodically lose and re-gain CDR lock 3. 0x4E device is setting as host to module. The eye diagram is as attached figures that meet 25G eye mask criteria…
hi,
Thank you for your response. in our real case i am not useing matlab gui , i will get the data in UART . how to separate the data for MRR and USRR objects data. Kindly clarify. The first subframe is MRR, while the second is USRR and how to identify…
Part Number: AFE7953 Other Parts Discussed in Thread: AFE7950 We are using AFE7953EVM module in our design. We do not have FTDI chip in our design so we can not control the AFE7953 directly with Latte Software. We want to program the AFE registers directly…
Other Parts Discussed in Thread: UNIFLASH , SYSCONFIG Tool/software: Code Composer Studio
TI DevTools (dev.ti.com) will be down for maintenance from Fri July 31 20:00 to 23:59 EDT (Sat Aug. 1 00:00 to 03:59 UTC).
During this maintenance window, Resource…
Yes, I can rump it at 0x4a.
root@j721e-evm:/opt/edgeai-gst-apps# i2cdump -f -y 0x5 0x4a
No size specified (using byte-data access)
0 1 2 3 4 5 6 7 8 9 a b c d e f 0123456789abcdef
00: b6 00 d1 00 00 00 00 00 00 00 ff 20 6c 00…