Part Number: EZ430-F2013 I am trying to work out what the actual point of the eZ430-F2013 dongle is.
I can understand the whole USB debugger + detachable target board thing, but this design seems pretty pointless to me (and yes, I do own one, but have…
Part Number: MSP430F2013 I know it can be done (even though the docs say it's not supported). I've configured it to work several times in the past. But I don't often use an MSP430 MCU and each time I pick it up again, I have a new computer and the old…
Other Parts Discussed in Thread: MSP430F2013 is there a driver etc. that will allow me to write to flash via the ez430-f2013 USB interface? I would like to give users the ability to customize the their display without exiting the user application.
T…
Other Parts Discussed in Thread: MSP430F2013 So one of the example projects for the ez430-f2013 is a flashing LED demo. It works fine, but I'm having trouble doing the same thing on Port 2. I connected an LED to P2 on the board, but it doesn't work…
I'm looking for the eZ430-F2013 or eZ430-F2012 Eagle footprint/schematic - see image (from SLAU176 ).
There only seems to be the Eagle schematics/board of eZ430-RF2500 online - see thread " ez430-RF2500 target board: any clearer PDF schematics…
Hi,
I wonder if you managed to connect ez430 with AFE221 usign SWD (I don't worry about UART).
I tried that and IAR debugger can't recognized MSP430FAFE221 using old ez430 board(4 pin connector).
When I connect MSP430F2013 (which comes with the…
I pulled an ez430-f2013 out to use in a lab project. I've had it for 5 years but only used it once under ccsv4. Under ccsv4 the device was properly detected during target debug. Using debug in ccsv6 (Version: 6.0.0.00190) the device is not recognized…
I just received my eZ430-F2013 USB emulator. I installed CCV 4.1.2. I tried the "First MSP430 Project" example on the Welcome Screen. My eZ430-F2013 emulator does not show up in the configuration file. The Driver is installed as MSP-430UIF. I…
Part Number: MSP430G2131 Other Parts Discussed in Thread: DRV8838EVM , DRV8838 , MSPWARE , MSP430WARE We are planning on using MSP430G2131 on DRV8838EVM. The datasheet for DRV8838 MCU mentions that to expand beyond the included firmware capability the MSP430…
Folk,
I've tried all the provided advice. As you can see from the attached screenshot. the ez430-F2013 is connected as COM3 with the correct drivers, and no other COM ports exist nor is any other COM software running. I've re-installed everything more…