Part Number: LAUNCHXL-CC1310 Other Parts Discussed in Thread: CC1310 Tool/software: Hi team,
Communication between CC1310 and Silicon Lab's SI4463, frequency: 433MHz, offset frequency: 20KHz, baud rate: 10kbps, two synchronization bytes, SI4463 sends…
Part Number: CC2640R2F Tool/software: hello
Is there a way to adjust the interval in the Smart RF Studio Continuous TX section?
Or, I wonder if it is possible to activate unmodulate in the packet TX part.
Currently, we need to measure the BLE communication…
Hi Mani, could you give us more details on the communication that you want to implement? Which communication pattern do you want to achieve? Which frequencies do you want to use? How many devices to you want to connect and which is there role? Which are the…
Part Number: LP-CC2652RB Tool/software: Can the "Socket" communications in the Smart RF Sniffer be used to send BLE sniffer data to a device with generic TCP socket communications? For example: an industrial PLC with Ethernet. If so, does the device…
Hi,
After checking with a colleague, here is some feedback:
If the temperature changes, you will need to re-calibrate the synth by issuing a CMD_FS . This command will always run if the device has been in Standby (even if you just call it once in your…
Part Number: MMWCAS-RF-EVM Other Parts Discussed in Thread: AWR2243 , Hi,
I'm trying to set up a connection between MMWCAS-RF-EVM (with 4 cascaded AWR2243) and another single-chip AWR2243 board. What I want to do is to use the cascaded board as a transmitter…
Part Number: CC1200 Tool/software: We are using CC1200 module, configured at 916MHz. As part of our testing, the PCBs with proper enclosure go through a thermal cycling test to verify any board level issue:
1. -35 to +55 degree Celsius with (3-degree…
Hi,
The connector is a MM5829-2700 from Murata (this information can be found within the design files of the LAUNCHXL-CC2640R2 - https://www.ti.com/lit/zip/swrc335 ) - I'll let you check the compatibility with the connectors you mentioned as I am not an…
Hello Community,
I am surprised that no one has answered my previous questions yet. I expect TI having RF application engineers who know how to use ICs made by TI. And my questions are very basic - needed for creating any RF link using Transceivers.
…
Hi Diego, Vincent informed me that you were working on reproducing our issue, have you been able to? My ticket with Vincent was closed without any warning, so I'm unable to communicate with him anymore.