Part Number: F28M35H52C Other Parts Discussed in Thread: SYSCONFIG , CONTROLSUITE Tool/software: Any available example to check CSM in the f28m35h52c chip ,I wanted to try for cortex m3, but all the examples of f2807x series are quite different, the have…
Part Number: F28M35H52C Other Parts Discussed in Thread: UNIFLASH , Tool/software: Hi
I use UniFlash to load the .out file for m3 core and c28 core of F28M35H52C. It always succeed when I load .out file for m3, However, when I try to load .out file…
Other Parts Discussed in Thread: UNIFLASH Tool/software: Master (M3) core. At some point after setting a Zone 1 password and the GRABSECT register to set sectors B-M to Zone 1, I am no longer able to access the device using the debugger, either with CCS…
Part Number: F28M35H52C Tool/software: Hi,
F28M35 frequently resets, and we can view the reset signal on the pins of ARS~ and XRS~, Why?
Maybe frequent resetting of the device causes that we can't program or erase flash. shown as below:
Here,…
Part Number: F28M35H52C Hello,
I'm trying to compile a code for F28M35H52C with TI v20.2.7.LTS having lots of linking problems
The same code has been always compiled with TI v4.9.9 without any problems.
Is TI v20.2.7.LTS compatible with the microcontroller…
Part Number: F28M35H52C Hi all,
I have a problem.
When I use sdo read access, I set a variable 'SdoSendNum4' to count the number of replies I should send.
I counted the number of sends and replies as equal to the number of requests read by SDO,…
Part Number: F28M35H52C Other Parts Discussed in Thread: UNIFLASH Hi,
I have a question。
After I modified the send function of can.c under f28m35 driverlib, I can't upgrade the compiled bin file。
Please help me solve the problem。
Part Number: F28M35H52C Hi,
We're working on F28M35H52C-based hardware development and planning to use UART0 for field firmware updates. Our problem here is that under current circumstances GPIO0 and GPIO1 are not available for UART0 as they're already…
Part Number: F28M35H52C Hello, i am using the driverlib and flashapi to develop a compact driver for the flash,
my program is executed from flash, however the entire driver is executed from ram (including flashapi and necessary flash functions)
the…