Part Number: F28M35M52C Hello,
We are using the Flash APIs in the F28M35M52C Concerto controllers.
We have configured the settings to access the Sector B in the .cmd file.
The sector B stores information which is required during firmware upgrade and…
Part Number: F28M35M52C I have a customer with the following situation thanks for your help:
We want to add the firmware upgrade functionality for the device. We would need support from TI in order to use the Flash APIs.
Issue faced:
The module doesn…
Part Number: F28M35M52C Other Parts Discussed in Thread: CONTROLSUITE
Hi,
I have some confusion about the value of the decoupling capacitors used for +1.8V internal regulator output pins. The section 8.9.1 "Analog Subsystem: Internal 1.8-V VREG", device…
Part Number: F28M35M52C After a redesign following pins are not used any more:
PH5_GPIO53 Pin 47
PH2_GPIO50 Pin 36
PH3_GPIO51 Pin 35
PJ1_GPIO57 Pin 62
ADC1INB0 Pin 117
ADC2INB0 Pin 136
For the above GPIOs the TRM is saying that default config is…
Part Number: F28M35M52C Other Parts Discussed in Thread: CCSTUDIO Tool/software: Code Composer Studio I've been trying to do software updates. For a few days I've not been able to connect to the TI repository:
http://software-dl.ti.com/dsps/dsps_public_sw…
Part Number: F28M35M52C Tool/software: Code Composer Studio I found a problem while debugging the circuit with ccs. The emulator can be connected to the M3 core and the downloader is debugged, but the emulator cannot be connected to the C28 core. Show…
Part Number: F28M35M52C Other Parts Discussed in Thread: UNIFLASH , Tool/software: Code Composer Studio Hi,
I am using the following post-build command to generate the BIN file from the OUT file. This command works, but the resulting BIN file produces a…
Part Number: F28M35M52C Tool/software: Code Composer Studio My problem, I'm testing two identical circuit boards, using the chip is the F28M35, one of which works and the other can't connect the emulator. I tested the circuit board that didn't work, the…
Part Number: F28M35M52C Tool/software: Code Composer Studio Hello,
I have a customized processor board and a XDS200 emulator. My software is demonstrated operational by flash programmed to the TI evaluation card by using the built-in emulator. Now I…
Part Number: F28M35M52C Other Parts Discussed in Thread: C2000WARE Tool/software: Code Composer Studio Hello,
I have control algorithm 2P2Z working and know how it can be mapped to PI control algorithm. However I want to increase the control update frequency…