Part Number: F28M36H33B2 I have a board using the F28M36 with two different Ethernet Phys. With the the two channel Phy I have no problems both running it through JTAG or without. For the single channel PHY I can run it fine with JTAG but if I run it…
Part Number: F28M36H33B2 I can connect to the C28x core on my concerto device but I cannot load a .out file. When loading into RAM it says "file load failed" and when loading into flash it says "Device may be operating in low-power mode". I have been…
Albert,
Albert Smit said: Is there a way that gui composer can load the program into RAM for both cores, M3 and C28?
Unfortunately this is currently not supported.
I think this issue is unique to running code on both cores of the F28M3x because…
Albert,
I have confirmation that this is a bug, all of these registers are there and available for use. I have submitted tickets for these issues to be corrected.
Regards, Cody
Part Number: F28M36H33B2 Tool/software: Code Composer Studio I am trying to create a Gui composer app that can view and graph data from my target and also log the viewed or streamed data by saving it to a CSV file. Basically the same as the example in…
Part Number: F28M36H33B2 I am trying to connect my cloud Gui composer app to the target via the USB-UART monitor. I have added the Serial_Cmd_Monitor.h and .c files to my project and added a UART communication in Target configurations on Com 4 where my…
Part Number: F28M36H33B2 Tool/software: Code Composer Studio I am trying to run my Gui Composer app as a standalone app. I have exported it and installed the runtime environment. When I run the Win32_start.bat file to start the app, it only shows the…
Part Number: F28M36H33B2 I am using the cloud based gui composer. If I preview the gui, it connects to the hardware via cloud agent and XDS 200 and programs the target, but then the target just hangs there and does not run. If it was running before I…
Part Number: F28M36H33B2 Tool/software: Code Composer Studio Hello,
NOTE: Please ignore part number in the post, this issue was seen on a product yet to be PG'ed.
During validation of security module we had a requirement to map the same .library…
Part Number: F28M36H33B2 Other Parts Discussed in Thread: UNIFLASH Tool/software: Code Composer Studio My post on this issue was locked but never resolved. Please see the previous thread:
I still have this problem. I can not get the debugger to connect…