Part Number: F28M36P63C2 Tool/software: hello,
We have a device that uses F28M36P63C2, we use the C2000 core to drive a motor, and the M3 core to do the external display and control. Once the customer reported that the indicator light of the equipment…
Part Number: F28M36P63C2 Other Parts Discussed in Thread: CCSTUDIO I failed to load the ccs project, the error is as follows
Error: Import failed for project '' because its meta-data cannot be interpreted. Please contact support.
the log file is…
Part Number: F28M36P63C2 Other Parts Discussed in Thread: TMS320F28388D , External EPI interface SRAM, its starting address is 0x300000. How can I write a program so that it is as convenient as using the internal memory of the device? And can dynamic…
Part Number: F28M36P63C2 Other Parts Discussed in Thread: TMS320F28388S , C2000WARE , CONTROLSUITE , Hi,
I need to know whether the below mentioned MCU is functional safety capable or not?......If it is capable means, please give the functional safety…
Part Number: F28M36P63C2 Other Parts Discussed in Thread: C2000WARE , CONTROLSUITE , Hello,
I am looking into the possibility of achieving SIL2 level of functional safety for our system which uses F28M36P63C2 microcontroller. Could you please give me…
Part Number: F28M36P63C2 The MII_PHYRSTn pin does not output a low level when the 3.3v power supply rises. Since the PHY, which is the output destination of MII_PHYRSTn, expects MII_PHYRSTn to be at a low level when the power supply rises, the initialization…
Part Number: F28M36P63C2 Hi Team,
There's an issue from the customer need your help:
Excuse me, I need to use the EPI HB16 mode in the red box in the above picture to access two chips, but the address line is only A0~A25. Can I use a GPIO to simulate…
Part Number: F28M36P63C2 Hi,
I am trying to read the logic low condition on an external peripheral using F28M36P63C2's GPIO12,13 and 14. There are no decaps on these pins but I am using an external 5K pull up with a 1500 pF filter cap on all these lines…
it appears we still have some in stock in TI store, and Mouser has 1 in stock
https://www.ti.com/product/F28M36P63C2#design-development
Yes, these tools are not being rebuilt. Once sold out they will be gone. All of the build files are provided…