Part Number: FDC2112 Other Parts Discussed in Thread: LDC1314 , LDC1312 , LDC1612 , LDC1614 Support Path: /Product/Development and troubleshooting/ I am using the FDC 2112 in single channel mode. I have the status config setup to return watchdog and amplitude…
Part Number: FDC2112 Dear expert,
My customer planning to add proximity sensing feature to Mobile Hotspot. The EE is similar to the picture as below.
Do you have some suggestion on how to design seseing coper pad? The Max sesing distance is 20cm
Product…
Hi Daivid,
There is no formula for detection range because it is system dependent. It is recommended to calibrate the detection range with your system.
Regards,
Yibo
Hi Jeison,
I am not aware of any touch slider device that provides a resistance change output. Our dedicated capacitive touch sensing devices all use a digital interface(I2C) for communication.
https://www.ti.com/compare-products/?id=3541&type=GPT&partList…
Other Parts Discussed in Thread: FDC2112 Hi,
I'm using FDC2112 to measure liquid level , download the software from TI. In folder "FDC2x14_LDC13xxRevB_LDC16xxRevB_EVM_Firmware_source", I can't find the ".project".
Thanks.. …
Other Parts Discussed in Thread: FDC2114EVM , FDC2114 Hi,
I bought a FDc2114evm board, can you give me a project which is using MSP430 control the FDC2114 directly ?
Using the GUI , I can't understand detailed .
Thank all
Other Parts Discussed in Thread: FDC2112 Hi,
I am currently working on a keypad for a customer, of which a FDC2112 proximity sensor is sought to be used, in the application note it is mentioned that for a single channel, a copper pour of 20,9 mm x 13,9…
Part Number: FDC2114-Q1 Other Parts Discussed in Thread: FDC1004 , FDC2112 , FDC2114 Dears
We are searching for the solutions for easy open trunk in automotive,and we recognized the reference design of FDC1004 and FDC2112/4.
But we heard that some bug of…
Other Parts Discussed in Thread: TMS320F28069 , FDC2112 Hi, we are developing a new project, using TMS320F28069 DSC which is connected to LDC1000 sensor through SPI and to FDC2112 sensor through I2C.
For both LDC1000 and FDC2112 interfacing, I'd like to…
Hi Rachel, sorry for the delay.
The 15 bits resolution datum comes from "FDC211x/FDC221x Current Consumption Estimator (Rev. A)" spreadsheet. The FDC2112 datasheet does not give complete insight into device operation, but if the input frequency…