Part Number: FUSION-DIGITAL-POWER-STUDIO Other Parts Discussed in Thread: UCD3138 I am using Fusion digital power studio of single phase PFC.
What was the gate driver circuit used in this?? How are the gate pulses given to the Mosfet generated.
Part Number: TPS53685 Hi,
I am looking into the usability of the TPS53685 with the AMD V3000 SoC and the web page of this DC/DC controller suggests the use of Fusion Digital Power Designer for the configuration of this DC/DC controller, but after installing…
Other Parts Discussed in Thread: UCD3138 Hello,
I have been trying to tune in Fusion Digital Power studio for the requirement of DC-DC PSFB converter (400V to 48V, 2.5kW ) requirement using UCD3138. I am able to get two situations where:
1. Stable PM and…
Part Number: UCD90124A When programmed with Version 7.7.1 of Fusion Digital Power Designer the EN and GPO are inverting from what is reported in the tool (Active High/Active Low) to what is actually witnessed physically at the pins of the device.
Was…
Part Number: UCD90120 Hi,
Which Fusion GUI and USB driver to the USB Interface Adapter will work with the UCD90120?
With 7.7.1, GPIO1 is not pulling high. With TI-Fusion-Digital-Power-Designer-2.0.179, GPIO1 is being pulled high. I am programming the NVRAM…
Part Number: FUSION-DIGITAL-POWER-STUDIO Hi,
How to use fusion digital power studio in offline mode?? What are the things that can be done in offline mode?? Also there is no firmware download option in offline mode, in the users guide they have shown…
Part Number: FUSION-DIGITAL-POWER-STUDIO Other Parts Discussed in Thread: UCD3138 , UCC28180 , UCC3818 Hi,
I want 230V Ac-400V Dc pfc circuit for 2Kw power rating.What are the changes that i need to make in fusion digital power studio of Single phase evm…
Hi Matteo,
You can access the tool from here: https://www.ti.com/tool/FUSION-DIGITAL-POWER-STUDIO
If you have any further questions on this tool or using the UCD31xx product family, please include the controller part number in the E2E so that the correct…
Part Number: TPS544C26EVM Other Parts Discussed in Thread: TPS544C26 Hi Team,
How to link TPS544C26 to Fusion Digital Power Designer?
I can't connect.
Below is the connection diagram and output voltage.
The following is the software operation interface…