Part Number: USB-PD-CHG-EVM-01 Other Parts Discussed in Thread: TPS25750 , BQ25798 Hi,
Before explaining the error situation, I would like to give some information about our circuit. Our ADCIN1 and ADCIN2 pins are supplied with 1.5V and cannot be changed…
Hello Jacques,
Glad the EVM is working for you now. Thanks for your feedback on it working on the desktop but not on the cloud GUI. We will make sure to look into that a bit more.
Let us know if you have any other issues.
Best Regards,
Justin Beigel
Part Number: FMC-ADC-ADAPTER Other Parts Discussed in Thread: ADS5263EVM Dear Sir or Madam,
Will the FMC-ADC-ADAPTER work with the ADS5263-EVM? The ADC is not listed on the flyer of the FMC-ADC-ADAPTER.
Best Regards,
Uros
Part Number: TUSB546EVM Other Parts Discussed in Thread: TPS65981 , USB2ANY I am likely to need further support beyond this specific inquiry, but I am having a great deal of difficulty trying to get FTDI adapters to work with this EVM and the tool "TPS65981_2_7_8…
Hi Jerome,
Jerome Beguin said: I still have a question. How are we suppose to setup the pull-up / pull-down resistor on the GPIOs.
Because some of them are also used for DSI configuration at boot. So should I keep the config for DSI lines or set up all…
Part Number: DIP-ADAPTER-EVM We are planning to use your evaluation board to validate a new fabrication process.
Is it possible to get access to the Gerber for the pastemask top layer?
We could work with any part of the layout file that shows the top…
Part Number: TDA4VM I tried to remove the following part in board-support/linux-5.4.106xxx/arch/arm64/boot/dts/ti/k3-j721e-vision-apps.dtso
- &main_i2c1 {
- status = "disabled";
- };
And run 'make linux-dtbs' in /opt/ti-processor-sdk-linux…
Release 07_03_00_07 is default to use UART2.
I plan to change it to MCU_UART0.
It is fails on J7200 EVM. Nothing shows from MCU UART.
But I could change it to UART0.
The same binary could not run on our hardware. Even nothing shows from UART0.
Are there…