Part Number: DRV8353RS-EVM Other Parts Discussed in Thread: DRV8353 Hi,
Please let me know, will DRV8353 chip fails if I connect and run 60 degree placed (instead of 120 deg) HALL sensor motor
From datasheet I could see DRV8353 supports 120 deg…
Part Number: DRV8353RS-EVM Other Parts Discussed in Thread: MOTORWARE , , DRV8353 I do not see a project Lab 11e for this kit in the Motorware files. How do I make one? I did all other labs that TI supplied to me for DRV8353RS-EVM. Now I need to spin…
Part Number: DRV5055EVM Other Parts Discussed in Thread: MSP-FET , DRV5055 , DRV5057 Hi all,
I have DRV5055EVM and I want to interface with it though any communication protocol with Tivac123gx. Is it possible and if yes, is MSP-FET required to establish…
Part Number: DRV8353 Other Parts Discussed in Thread: MOTORWARE Tool/software: Code Composer Studio How to use DRV8353- EVM kit with sinusoidal drive and 3 Hall sensor inputs from motor?
Part Number: DRV5032-SOLAR-EVM Other Parts Discussed in Thread: DRV5032 , DRV5053 Dear Sirs, I receved your DRV5032 Ultra-Low Power, 1.65V to 5.5V Hall Effect Switch Sensor Evaluation Module but I’m not scure if it can be helpfull for me. I need to mesure…
Other Parts Discussed in Thread: DRV8307EVM Hi,
My customer tries to operate motor with DRV8307EVM. They use the hall element. it is "HW-105W". VM=24V.
At this case, What are we select at JP3 and JP4? I think think that we select the following. Is…
Other Parts Discussed in Thread: MOTORWARE , DRV8301 hi I use the DRV8301HC -C2 -KIT , I Have been testing PROGRAM (lab ) in motorWare .now I want to turn my motor PMSM with Hall effect sensor . what program should be used to control suite, (it is sensord…
Hey Francois,
The DRV8363-Q1 EVM was built for compatibility with LAUNCHXL-F280049C. In one of our initial revisions we had challenge running HALL C to J9.17.
The Hall signal would not toggle which affected Hall based commutation. Therefore, We…
Hi Henry,
Thank you for your interest in the DRV8353R EVM.
You are correct, unfortunately this board only supplies 3.3V to the hall power.
The DRV8353 Device itself will work just fine with this motor, but unfortunately the board was designed without…