THX
So then if optoisolators are not going to work with UCC25660x.Then How would i design a optocoupler FB for my circuit?
I also plan to have a Hall effect sensor for over current protection ( i am also open to other types like shunt + INA IC and other…
Part Number: FDC2214 Other Parts Discussed in Thread: FDC1004 Tool/software: I have design challenge to make the LED camp with the human hand detection. Requirement mention below.
LED lamp has close body which is cover by the plastic part so no external…
Hello Tom,
Thank you for your post.
I am most familiar with the magnetic sensing for motor encoding.
Have you taken a look at this reference design? Abs. Angle Encoder Ref. Des. W/ Hall-Effect Sensors for Precise Motor Pos. Cont. (ti.com)
Here is also…
Ryder,
Here is a link to our hall based current sensor solutions that can be used to replace a shunt. If you use a hall based sensor, than you no longer need the amplifiers in the DRV8353. I would then recommend a DRV8350 (no current shunt amplifiers) instead…
Dear Yara Thank you for your answer.
1. I have a product designed with DRV8316CR. I was in trouble because I couldn't use two functions at the same time. DRV8376 is good. But it is not available for purchase yet. Please let me know when it will be available…
Part Number: MCT8316A Other Parts Discussed in Thread: MCT8315A Tool/software: Hi,
Short background:
Till the new design which is in the pipeline we used to use DC brush motors or BLDC with hall effect.
In the production line we test the power stage…
Hi PY,
Thanks for posting to the Sensors forum.
The TMAG6180-Q1 has documentation to aid ISO 26262 system design up to ASIL B. This documentation can be requested via the device product page.
The TMAG5170-Q1 and TMAG5173-Q1 have systematic capability…
Hi Julien,
Thanks for posting your question to the sensors forum and welcome to E2E.
The BOP min/max and BRP min/max specs are provided to account for device variations across supply voltage and temperature. And best practice is to design the system around…
Rifa,
The CC2340R5 requires an external filter that is used by our reference design. This filter is comprised of L33, C33 and C34 as shown in your screenshot.
The filter reduces the harmonic content of the output of the PA and is closely matched to 50Ω…
Part Number: LAUNCHXL-F280049C Tool/software: Hello,
I am working of an inverter design using your tiduay6e appliction report. We are having some difficulties in implementing the Build level 2 and build level 3, hence I would need some clarification on…