Part Number: MMWCAS-DSP-EVM I am setting up an advance framing and after I send the AWR FRAMESTARTSTOP CONF SB, I get two errors:
1) - AWR_AE_MSS_RFERROR_STATUS_SB - with ERROR_STATUS_FLAG set to 1 (BSS FW assert)
2) - AWR_AE_RF_CPUFAULT_SB - with…
Part Number: MMWCAS-RF-EVM Other Parts Discussed in Thread: MMWCAS-DSP-EVM , Hi there,
I am currently using the MMWCAS-RF-EVM along with the MMWCAS-DSP-EVM. I was wondering if it was possible to somehow trigger a signal or a pulse of some sort (perhaps…
Part Number: TDC7201-ZAX-EVM Other Parts Discussed in Thread: TDC7201 I installed the GUI software, inserted TDC7201 module into MSP430 module, and got the result of read all no errors under DEBUG,as shown in the figure. However, when I access the start…
Part Number: DRV5055EVM Other Parts Discussed in Thread: MSP-FET , DRV5055 , DRV5057 Hi all,
I have DRV5055EVM and I want to interface with it though any communication protocol with Tivac123gx. Is it possible and if yes, is MSP-FET required to establish…
Part Number: DRV8353 Other Parts Discussed in Thread: MOTORWARE Tool/software: Code Composer Studio How to use DRV8353- EVM kit with sinusoidal drive and 3 Hall sensor inputs from motor?
Part Number: DLP6500FYE I am working with a DLP Lightcraft 6500 EVM device running in "on-the-fly" pattern mode. I give the device a series of binary patterns, and then I use an external trigger to advance the frames. After receiving each trigger, the…
Part Number: DRV5032-SOLAR-EVM Other Parts Discussed in Thread: DRV5032 , DRV5053 Dear Sirs, I receved your DRV5032 Ultra-Low Power, 1.65V to 5.5V Hall Effect Switch Sensor Evaluation Module but I’m not scure if it can be helpfull for me. I need to mesure…
Part Number: DLPC900 I am currently working with the DLP Lightcraft 9000 device and will be using it on ''Pattern-on-the -fly'' mode, where I will be uploading some binary patterns.
The module needs to be synchronized with a camera. My question would…
Other Parts Discussed in Thread: DLP3010 I want to get the signal from the trigger out2 when the dlp3010 project patterns we set in advanced,the setting of the software is attached.
Its weird that the function generator displayed 3.3v whether we project…
Part Number: DLPDLCR4710EVM-G2 Other Parts Discussed in Thread: DLPC3479 Hi,
We are currently checking out all the resources available on the device and we are wondering if it is posible to enable-disable the DMD using an external signal (while in …