Part Number: HD3SS3212 Can I use HD3SS3212 to switch Aurora (Xlinx fast Transcivers - like CML) at 10Gbps or 6.25Gbps? If it possible, can you suggest how connect HD3SS3212 to FPGA
Part Number: HD3SS3212 signal definition by Xlinx
The Aurora 8B/10B protocol uses differential signaling between ports. This section specifies signals using peak-to-peak differential voltages. . Each signal swings between A volts and B volts. Using these…
Part Number: TPS25831-Q1 Other Parts Discussed in Thread: HD3SS3212-Q1 , HD3SS3212 , TPS25830-Q1
Hi E2E team,
I would like to use TPS25831-Q1 and HD3SS3212-Q1 to implement an automotive product. A simplified block diagram is shown below:
And Its planning…
Part Number: HD3SS3212 Hi,
I am planning to use this MUX or De-MUX for my USB Type-C application. In the datasheet it is mentioned "In the case where the common mode voltage in the system is higher than 2 V, the coupling capacitors are placed on both…
Part Number: HD3SS3212 Other Parts Discussed in Thread: HD3SS3202 Hello,
In another E2E thread, I saw that the insertion loss, cross talk, return loss, and off isolation specs are different between the two devices. However, when comparing the devices…
Part Number: HD3SS3212-Q1 Other Parts Discussed in Thread: DP83TC812R-Q1 Hi team,
Can HD3SS3212-Q1 support RGMII signal? If so, is it necessary to add AC couple capacitors?
BRs,
Haury
Part Number: HD3SS3212-Q1 Other Parts Discussed in Thread: HD3SS3212 , DS90UB949A-Q1 Hi Team,
This schematic's application is automotive IVI system. Please check it and let me know the review result.
Schematic_HD3SS3212.pdf
Regards,
Good idea!
I consider this case closed as of now as I cannot get any more help and new boards are on the way. If necessay I open a new case here on the forum.
Thanks for all the help!
Björn