Part Number: HDC1010 We are trying to measure the temperature of a copper area on our board which is electrically isolated from any other circuit. Should we just run a copper bit under the body of the sensor to get this measurement?
Part Number: HDC1010 Hey Team,
Dan is working with our HDC1010 and STM32F407. He's configured the I2C interface to run at 14kHz, SM mode. Dan is using the following sequence to read the sensor:
Write sensor configuration: x80/x02/x10/x00
Write…
Part Number: HDC1010
Dear all,
I cant read the data from HDC1010. I have attached the Schematic and board layout. kindly give me the solution.Initially 1.5K pull up connected to the scl and sda this time not working. Then Pullup changed to 10k this…
Part Number: HDC1010 Hi Team,
I am using TI HDC1010 temperature sensor, I have interfaced with our MCU (MCU+BLE) and still, the chip is not active. Please, someone, share the working schematic with supported firmware to test my board.
Regards Kum…
Part Number: HDC1010HDC1010 support,
Is there a document that provides a recommended routine for using the heater to recondition the humidity sensor? For example, how long should it be on? How often can it be turned on? Any other guidance?
Thanks…
Part Number: HDC1010 Other Parts Discussed in Thread: HDC1000 , Hello,
I am developing a mikroe addon board with a HDC1000 IC on it:
https://www.mikroe.com/hdc1000-click
I already have a very good working driver for this click board on my PIC platform…
Part Number: HDC1010 Other Parts Discussed in Thread: HDC2010 , SYSCONFIG , HDC2080 Hi,
I am trying to read the temperature and humidity data from HDC1010. Is there any library or example written with C code ?
Any advise ?
Part Number: HDC1010 Other Parts Discussed in Thread: HDC1000
Dear Sirs,
May I use same code for HDC1000 and HDC1010 if I upgrade to HDC1010 from HDC1000?
Thanks.
Part Number: HDC1010 Other Parts Discussed in Thread: TDC1000 Hello,
Can The HDC1010 sensor work in mediums other than air? In that case, does the calibration need to be adjusted?
What are the main parameters that affect the drift of the accuracy…
Part Number: HDC1010 Dear Sir,
Please you kindly review below picture, my customer was use HDC1010 measure Humidity(RH%) data compare with machine value have arround 7% error.
Please you kindly review and help provide advise.
Thanks!
Steven