Part Number: HDC1080 I have an Artix7 FPGA connected to HDC1080. I am using Microblaze withe the Xilinx AXI IIC IP to read data from the sensor. But the HDC1080 doest not ACK the slave address.
I have checked the sensor supply is Okay and both the SCL…
Part Number: HDC1080
While continuously reading temp/humidity, only the high byte changes — the low temperature byte and the humidity value remain unchanged. What might be the reason? Image attached below. The bus speed is 100 kHz, and the conversion…
Part Number: HDC1080 Other Parts Discussed in Thread: HDC3020 Hello Experts ,
Please refer to below issue and guide me to come out of this issue.
Reference humidity measured by the integrator: 45.3% RH
Humidity measured by the PCB: 0% RH
Reported…
Part Number: HDC1080 Hi Team,
The system is designed for indoor use, with only the enclosure assembled and no internal heat-generating components.
The enclosure already includes a sensing opening to allow the temperature and humidity sensor to detect…
Part Number: HDC1080 Tool/software: I've configured my HDC1x and tried reading from it, but I can't read from the temperature or humidity registers, what's wrong?
Part Number: HDC1080 The datasheet says that this pad should not be tied to any net. It also doesn't even definitely say that it should be soldered. Does this pad serve any purpose, such as contributing to measurement stability? Is there any drawback…
Part Number: HDC1080 Tool/software: Hello dear
I work for a medium-sized company Elkoep.s,r,o on the development of electronic devices for households. We often use your HDC1080 temperature and humidity sensors for products. In the production process…
Part Number: HDC1080 Other Parts Discussed in Thread: HDC3020 , HDC3022
Hello,
I have a question regarding the long-term stability of the HDC1080.
We are using HDC1080 in a gas dew point sensing application.
At the time of production and initial…
Part Number: HDC1080 Hi Team,
Customer would like to evaluate their humidity sensing accuracy in the system, the requirement is 3%, and datasheet only shows the typical value is 2%.
Could you please help provide the min & max accuracy here for customer…