Part Number: HDC2010 Hi Team,
could you help to know how we should utilize heater function depending on external environment?
- what event/output data result should trigger the heater on?
- what event/ output data result should trigger the heater off…
Part Number: LPSTK-CC1352R Other Parts Discussed in Thread: HDC2080 , HDC2010 , I was trying to get data from HDC2080 sensor with use #include <ti/common/sail/hdc2010/hdc2010.h> driver but my code was hanging up after write I2C frame was sended.
To verify…
Part Number: HDC2010 Other Parts Discussed in Thread: HDC2080 Hello Everyone
We develop an roomthermostat with an HDC2010, we have about 100 ore more prototypes.
We use the HDC in Automeasurement Mode both(humidity and temperature) in 14bit, 1 sampe per…
Part Number: HDC2010 Hi Sir,
Our customers reported that the temperature and humidity measured by HDC2010 has a large deviation. Comparing the value measured by the calibration instrument with the data directly monitored by HDC2010, it is found that…
Part Number: HDC2010 Hi,
when customer is testing HDC2010, they found it work at self-heating, temperature read as 70℃, it recover until reset IC.
Address 0x0E=0x50, "heater on" is off.
and the test environment is as below:
temp: around 55℃ …
Part Number: HDC2010 I'm using the HDC2010 installed on the BASSENSORS Booster Pack, on a Tiva TM4C board.
Through I2C I can set and read back all of the 2010's registers. I verified that the manufacturer ID and the part ID numbers are correct, too…
Part Number: HDC2010 Other Parts Discussed in Thread: HDC2022 hi:
Hdc2010 is used in IPx4 waterproof structure.
Because it is waterproof, it exists in closed space.
The air enters into the structure through waterproof and breathable membrane (IP54 standard…
Part Number: HDC2010 Hi expert,
My customer has question from the datasheet, there's a parameter called "IDDHEAT".
There's a description only mentioned that operating at -40~85 degree. But we are not able to understand this parameter is…
Part Number: HDC2010 Hi expert,
TI don't recommend rework HDC2010 from datasheet description 10.1.1.3 Rework.
Could you please give me your advice for the following cases?
1. If customer will find the assemble issue on HDC2010. They would like to…
Part Number: HDC2010 Other Parts Discussed in Thread: HDC3020 Hello,
I was wondering if the NIST traceability only applied to the temperature sensing component of this device or if it also meets NIST relative humidity tracing. I couldn't find anything…