Part Number: HDC2010EVM I have followed the directions in the user guide for installation several times now. It never begins the driver installation wizard and therefore it will not connect with the eval board. Is there a separate download link or can…
Other Parts Discussed in Thread: HDC2010EVM , FDC2214EVM Hello support team,
Can HDC2010EVM run on Windows 10 using the latest version of Sensing Solutions EVM GUI - 1.9.4?
According to the user's guide of HDC2010EVM, it is stated that "Sensing Solutions…
Part Number: HDC2010EVM Other Parts Discussed in Thread: HDC2010 Hello E2E,
Our customer have two EVM. They are evaluating now them. However, two EVMs output data are not look like for normaly.
No.1-EVM; At over 60-% humidity, the output data is less than…
Part Number: HDC2010EVM Hello E2E,
Our customer have two EVM. They are evaluating now them. However, two EVMs output data are not look like for normaly.
No.1-EVM; At over 60-% humidity, the output data is less than ambient. Please see the Humidity.pdf …
Part Number: HDC2010EVM Other Parts Discussed in Thread: HDC2010 Hi
Question:
Can the EVM GUI with HDC2010EVM be used also with a sensor (HDC2010) with the "other" ADDR (namely 1000001) ? the HDC2010 arrives with ADDR 1000000 (ADDR node connected…
Part Number: HDC2010EVM Other Parts Discussed in Thread: HDC2010 I am currently working to read the HDC2010 EVM chip using both an Arduino and an Atmel microcontroller, and the temperature readings are about 20 degrees Fahrenheit too high on both boards…
Part Number: HDC2010EVM Other Parts Discussed in Thread: HDC2010 Hello,
Regarding to HDC2010 EVM, my customer is asking some question.
To evolution, they will design with EVM + their original PC application (for example EXCEL macro).
Sensing Solutions…
Hi Maynard,
Thank you for providing the images. From the images, it looks like you are trying to connect a HDC1010 device to a HDC2010EVM. These devices are not pin compatible. This is probably why it isn't connecting to the GUI.
Regards, Pavani T…
Hi Fisher
For HDC2010EVM, the installation issue is not solved after I tried to go through the steps from this thread: https://e2e.ti.com/support/sensors/f/1023/t/681030?HDC2010EVM-Driver-installation-issue
There are some steps are different:
Open "Device…
I've used both the in browser and the local downloadable GUI. My laptop is also set to stay powered on while it is plugged in. What I have since noticed is that the USB connection is being dropped after an unspecified time. I switched to a powered USB…