Hi CELESTE GONZALEZ CANTERO,
Please review section 6.3 in the document we linked to earlier, A Basic Guide to Bridge Measurements. This is effectively the system I believe you have, and this section explains in more detail what I am referring to
When…
Other Parts Discussed in Thread: HSMC-ADC-BRIDGE I am trying to use a ADS41XX/58B18EVM board with an Altera MAX 10M50D Evaluation board, though a HSMC-ADC-BRIDGE Rev. C1 interface board.
The positive and negative LVDS pins seem to be switched around. …
Other Parts Discussed in Thread: ADS42LB69 , ADS42LB49
I need to interconnect ADS42LB69 EVM with Arria V FPGA development kit ( www.altera.com/.../kit-arria-v-gx.html) from Altera. Arria V FPGA kit has HSMC connector on it. I need to use both the ADC channels…
Hi nestor Garcia,
There are a couple of resources available regarding temperature measurement. They are A Basic Guide to RTD Measurements and A Basic Guide to Thermocouple Measurements . There is also a Temperature Sensing Code Library that may be useful…
Hi Eduard Dubinin,
Bob is out of the office this week so I will offer my support while he is gone
Can you tell me if the buffer is enabled for your measurements? With the buffer disabled, the ADC input impedance will be typically 39kohm at a gain of 128…
Other Parts Discussed in Thread: HSMC-ADC-BRIDGE , ADS4249 , ADS4249EVM Hi,
I'd like to ask for information about "HSMC-ADC-BRIDGE REV C".
Concretely, I need one about pins information.
Although I confirmed the schematic file about the product…
Hi Nimit Vachhani,
A couple of questions / comments about the schematic:
You show both a GND net and an AVSS net - are these connected somewhere?
You have a lowpass filter on your inputs (S+ / S- pins) but not on the SENSE lines. Instead you only have…
Hi Mike N
Can you send us the data you are seeing in an Excel file? Preferably the raw ADC data?
It would be useful to see both the "good" data using the 1kohm bridge and the "bad" data using the 10kohm bridge so we can compare
-B…
Hi Shkelqim,
If I understood correctly, your bridge offers full-scale signal of +/- 20mV. The ADC for weight scales device you feature above, from another manufacturer, already integrates a programmable gain amplifier (PGA). According to your equation…
Patrick,
I will look into this for you. Did you order the HSMC-ADC-BRIDGE card? When you mention "Does not work" can you tell me what the issue was?
Regards,
Jim