F280200 has UL/IEC60730 compliance. Please refer to IEC60730SWPACKAGES Driver or library | TI.com . There’s a VDE letter in the software package. Please refer to https://www.ti.com/lit/spruhi3 as well
Sirs, My customer also requested the same one. IEC60730SWPACKAGES for TMS320F2837xD. Is it available if I ask TIer by an e-mail ? * It is not available in TI-HP. www.ti.com/.../iec60730swpackages
Graham,
The need to check the SRAM at power up(POST type test) is really dependent on the end application requirements for any health checks before the MCU begins controlling the system.
As you mention the SRAM(as well as other memory like Flash/ROM…
Frank,
For the F28335 device you can download this SW package: http://www.ti.com/tool/IEC60730SWPACKAGES
There should be a SRAM test, based on the March13n algo. This should provide superior fault coverage to "GALPAT" type tests. Let me know if you…
Part Number: TMS320F28377D Other Parts Discussed in Thread: IEC60730SWPACKAGES Hello,
Me and my customer are studying 'IEC60730 Safety library', that is, IEC60730SWPACKAGES http://www.ti.com/tool/IEC60730SWPACKAGES
I hope you have the spec IEC60730…
Part Number: TMS320F28377D Other Parts Discussed in Thread: IEC60730SWPACKAGES Hello,
Could you please advise how to obtain the titled document?
The doc# is referred in [Self_Test_Application_Users_Guide-1.00.00.00.pdf] / C2000-DIAGNOSTIC-SW-PACKAGE…
Zaw, We do not have anything specifically for the 281x. However, this library and the APIs for the F2802x device can help: www.ti.com/.../IEC60730SWPACKAGES While the examples are built for a newer device (I suggest looking at F2802x), you should be able…
Sam,
We have RAM tests packaged with other module tests in a IEC60730 package here http://www.ti.com/tool/IEC60730SWPACKAGES . This support the F2806x.
For a run time environment customer can choose which RAMs to place under test; so they would…