Part Number: INA122 Other Parts Discussed in Thread: INA326 , , INA114 , INA500 , PSPICE-FOR-TI , INA121 , INA118 , INA128 , TL7660 Tool/software: Hello
I am trying to figure out a way to measure current from an electrolytic cell. The potential difference (as…
Part Number: INA186-Q1 Other Parts Discussed in Thread: INA121 Tool/software: Hi Team,
Could you please share some suggestion for selecting a suitable current sensor and shunt resistor?
1. Detect 0~100uA current, accuracy is 1uA(whole temperature range…
Part Number: INA121 Other Parts Discussed in Thread: TINA-TI ,
Tool/software: TINA-TI or Spice Models
When run TI-TINA to simulate a simple setup bases on INA121 I get strange signal distortion and it seems to depend on temperature as well; See attached…
Part Number: TL071A Other Parts Discussed in Thread: TL072B , INA121 , TL072A , TLC2202 , LM675 , Hi,
Our customer is considering using TI's OPAMP under vacuum about 10^-4Pa. Is it okay to use it? Is this kind of test conducted in reliability testing? (As…
Part Number: INA121 NO DATA SHEETS MENTION , OR QUANTIFY AMPLITUDE PHASE SHIFT
ALL PHASE SHIFT/TIMING IS RELATED TO FREQUENCY PHASE SHIFT
I NEED TO BE ABLE TO SELECT THE BEST INSTRUMENT AMP AND OP-AMP THAT HAS THE LEAST AMPLITUDE PHASE SHIFT
OR-- THE…
Part Number: INA114 Other Parts Discussed in Thread: INA121 , INA828 Hi
I have an application here I get a voltage measurement to be done at pins of a resistor of 300K powered by a fixed current source
The voltage maximum will be 0 to 10V
I must of course…
Part Number: INA121 Other Parts Discussed in Thread: OPA547 Do you have radiation data for the INA121U?
If not, could you provide the die area?
This would be used to predict susceptibility to
radiation.
Thanks,
Carolyn Sleeper
Hi Daveon
The schematic diagram and layout are as attached.
Signal>INA121+DS1882 Amplification>PCM6260
The question is as follows
1. They have problems with 0~20db recording under Micbias 5v ~9v and high swing.
2.There will be noise when the…
Part Number: INA121 Hi,
I am using INA121U for my design and would like get some clarification on using the Offset Voltage specification in the datasheet.
The first page of datasheet provides "LOW INPUT OFFSET VOLTAGE: ±200uV". For what gain and temperature…
Part Number: INA116 Other Parts Discussed in Thread: OPA928 , INA819 , , INA121 Hello
I am using your instrumentation IC INA 116 inputs pins are connected to the output of EMCO DC TO High voltage DC convertors I need to replace this IC as this part is not…