Part Number: INA126 Other Parts Discussed in Thread: OP27 Hi,
I am using INA126 with the GAIN of 368 (RG = 220 Ohms). Input to the ref pin is about 6.5 VDC. My output oscillates withing 6 mv ! However, when I change my RG to say 500 Ohms (lesser GAIN…
Part Number: INA126 Other Parts Discussed in Thread: OPA627 , THS4531A , NE5534A , NE5534 , LM317
Hello
My customer had chosen INA126 for their product ( Flow-meter) but they found noise issue for 1pcs of 2500 pcs in their production line.
Where: Vs…
Part Number: INA126 Other Parts Discussed in Thread: INA122 , , INA326 Hi,
I need to amplify a pyrheliometer signal ranging from 0 to 10mv, in the range of an STM32F429ZI ADC that is 0 to 3.3V .
We already have produced some PCB where we have a single 5V…
Part Number: INA126 Dear Sir/Madam,
I am evaluating on TI INA126UAG4.
Below showing the connection where Vin- is connected to GND and Vin+ to 1.0V external supply. I am using Rgain resistor of 75K and based on calculation, the G should be 6.06 which means…
Part Number: INA126 I uses the INA126 to amplify a high side current sense resistor (0.01ohm).
In my test the Vload is 1.03V
The load is 90ohm
the V(rsense) is 170uV
the gain resistance RG is 34ohm -> gain = 2357
The INA126 output is 33mV -> Gain…
Part Number: INA126
Hi. I am having problems to use INA126 with load cell. My configuration is: Input common mode Voltage = 2.5V. Power Supply = 5V/0V. Vref = 0V. I would like to know the limits of Output Voltage I will have.
For example, on the picture…
Part Number: INA126 Other Parts Discussed in Thread: INA122 , , ADS1115 , LM7705 , OPA320 I've got a 2 wire pyranometer. It generates voltage 0-40mV based on the strength of the solar irradiation.
I've got in my toolbox INA126 and INA122.
Are they…
Hi Peter,
I just wondered how you are getting on with solving this riddle. While I was waiting, I tried three things out :-
1) Going back to using INA126 on its own
2) Connecting OPA2192 to INA126
3) Trying INA163 on its own
Here's what I found ;-…
Part Number: INA126 What is the input range of INA126 .How small can be the Δ V so that i get a reasonable good output. Is Δ V =.5mv be good enough.
And also what is a good method to reduce noise, because when my hand comes near the circuit…