Part Number: INA168 Hello guys,
One of my customers is considering using INA168 for their new products.
They want to know what the maximum value of total output error at all temperature range is to assume the worst case.
But it can't be found in the device…
Part Number: INA168 Hello guys.
One of my customers is considering using INA168 for their new products,
They have the following question about INA168. Could you please give me your reply?
Q, What is the maximum capacitor can be connected between "OUT…
Hi Angel,
Because it would be great if it worked, given its very attractive price point and excellent CMRR
I thought the point of placing the amplifier post LC filter was that the fast-switching dv/dt signals were gone. Specifically, SLYA031 says: "After…
Part Number: INA168 Hello, sir
Circuit :
Input - 20-50V LED converter (especiallay, with 120Hz Current noise)
load - LED 70mA - 3A
Sensing R - 60m ohm
RL = 60.4k // 1uF
VCC - 5V
Result :
ILOAD0 - UNIT FUNCTION 50V after 10msec
Output at OUT PIN : It…
Part Number: INA168 Other Parts Discussed in Thread: TINA-TI , INA193 We are using this to monitor the current in a battery system. This is a unique battery that is "triggered" to provide voltage, i.e., it is not on all the time and switched on and off…
Part Number: AMC7812 Other Parts Discussed in Thread: INA168 , Hi, there is a problem when I use INA168 and AMC7812. There is a 400-500mV voltage in the ADC single-end input port (CH0) when the sampling voltage is zero. In this situation, there is only…
Hi Manuel, thank you for your interest and your time.
The INA170 looks ideal for my project and i will order a few devilces to start making test in the lab.
The overall process of the project is going well.
Regarding the INA168, i will manage to get…
Part Number: INA183 Other Parts Discussed in Thread: INA138 , INA139 , INA169 , INA168 Hi team,
The output signal of INA183 is voltage, do we have device with current output propotional to sensed voltage?
Nison
Part Number: INA168 Other Parts Discussed in Thread: TINA-TI Hello,
is the bias current of the INA168 always sinked into the device (in datasheet as positive), or is it possible that e.g. at low VCM also a current is sources by the IC?