Part Number: INA180 Dear Sir or Madam,
Could you inform me about terminal finish of the part INA180A1QDBVRQ1. Could you tell me the thickness of Au in case the terminal finish is NiPdAu or NiAu or Au.
Could you tell me ECCN (Export Control Classification…
Part Number: INA180 Other Parts Discussed in Thread: OPA2365 , OPA365 , INA296B , INA240 Hi all
I was doing some simulation about low side current sensing circuit using high speed opamp and current sense amplifiers. Since INA180 has high market rank i decided…
Part Number: INA180 I am utilizing the INA180 for monitoring DCDC current. The INA180 amplifies the voltage across the current sensing resistor, presenting a sine wave pattern as observed on the oscilloscope. Consequently, despite a stable output current…
Part Number: INA180-Q1 Hi Experts,
ZXCT1110QW5-7 is mass production in customer. Could you help to provide Pin-To-Pin device to replace ZXCT1110QW5-7? Thanks.
Best Regards
Songzhen Guo
Part Number: INA180-Q1 Hi,
Could you give the formula for getting current flowing through Rsense by output voltage of the current-sense amplifier.
I'm using INA180A2QDBVRQ1 in my design. In the data sheet it's mentioned the gain error factor and gain…
Part Number: INA180 Hi all,
Customer now used INA180B3 do the current sensing with shunt resistor(1mOhm)
Schematic and waveform is followed below.
The distortion and wrong current sensing ratio maybe is cause by the resistor divider which added by customer…
Part Number: INA180 Other Parts Discussed in Thread: INA168 , INA240 Hi!
I have been investigating ways to measure loudspeaker current connected in a bridge-tied-load fashion to a class D amplifier.
Following the excellent SLYA031, I have decided on placing…
Part Number: INA180 Hi,
The input voltage range is 2.7V-5.5V in INA180, normal number is 5V.
Will there are any performance influence when I supply the device with 3.3V
Thanks
Yishan Chen
Part Number: INA180 Hi,
I am designing a controller as shown in the block diagram below. I am using low side current sensing with INA180. Max Current is 20A and sense resistor used is 0.002ohms.
Will there be any issue for sensing DC Input current if ground…
Part Number: INA180-Q1 Hi there,
Could you tell me Moisture Sensitivity Level (MSL) of the part INA180A1QDBVRQ1.
Thanks.
Best Regards,
Kaoutar Ben Kaddour