Part Number: INA185 Hi
My customer had a defect as follows.
When VS(#6) is turned on/off, a spike voltage appears in OUT(#1)
Didn't connect any other pins.
Input: DC Supply (2.8V)
Waveform: Ch1(yellow): VS , Ch2(green)_OUT
( customer measured…
Part Number: INA185 Other Parts Discussed in Thread: THS4521 , TINA-TI
In order to use the 16-bit mode of F28379D ADC, I would like to use 2 INA185 connected in reverse (VDD = 3V, output signals are biased to 1.5V) to create a differential signal…
Part Number: INA185
Hello Sir/Ma'am,
We have built the prototype circuit of the INA185A3IDRLR current sense amplifier on the general-purpose board for our design testing & validation.
We design this circuit to work in low side sensing configuratiion…
Part Number: INA185 Other Parts Discussed in Thread: INA196 Can this device be used in a 4-20ma current loop instrumentation measurement application? Has anyone done this? If so can you share your experience and any info?
Part Number: INA185
Hello
We are using the following TI parts for our application.
1) INA185A2IDRLT
2) ADS1118IDGSR
3) TMUX1108PWR
4) TMUX1104DGSR
5) TXB0108PWR
We design this circuit for a precision current monitoring application…
Part Number: INA185 Hi Sir
When INA185 work on unidirection mode ,if in this mode have reverse current ,what's the maximum voltage that INA185 can support
Part Number: INA185 Other Parts Discussed in Thread: INA240 Hi,
This may be a silly question. I'm using an INA185A2 current sense amplifier for in-line current sensing in a BLDC application. Vsupply is 3.3V with a 1.65Vref from a voltage divider.
…
Part Number: INA185 Other Parts Discussed in Thread: INA351 , INA181 , , INA281 , INA213 , INA191 , INA190
Dear Community,
We're working on 2 highly cost-sensitive application use cases where we have to measure the voltage drop across a Resistor connected…
Part Number: INA185 Other Parts Discussed in Thread: TLV3201 , , OPA2810
Hi Team,
Our customer would like to confirm if the devices below are multi-component semiconductor (MCO). I have confirmed that these devices are single die but are they MCO…
Part Number: INA185 Other Parts Discussed in Thread: INA210 , INA190 Hi Team,
The customer wants to measure currents in the range of 1uA to 1A, with an accuracy of 1uA. Could the INA185 or the INA210 be able to reliably amplify voltages from 1uV to…