Part Number: INA186-Q1 Hello Team,
Could you kindly share us the ESD report of INA186-Q1?
Also could you share the ESD test setup or which test condition standard should we refer?
Many thanks!
BR
Frank
Part Number: INA186-Q1 Other Parts Discussed in Thread: INA186 hello,
I have one question regarding the INA186A1QDCKRQ1 usage like the picture. We set the GND at the positive of shunt. That means that the potential of the shunt negative will be lower than…
Part Number: INA186 Hi
The Rf in the input side, if will affect accuracy or it can improve noise performance?
Do we have the general application note for Cf design or typical design?
Part Number: INA186 Hi
My customer need to improve the INA186 output noise, because the waveform seems too bug to affects the stability of trigger point.
Do you have any suggestion to reduce noise for output?
Part Number: INA186 Other Parts Discussed in Thread: INA241A , INA190
Dear Technical Support Team,
I have been searching -2V VCM capable similar to INA186.
Could you introduce it?
Rsense=82Ω and bidirectional.
Best Regards,
ttd
Part Number: INA186 Hi Team,
My customer is going to use INA186A3IYFDR. However, there are two different package spec in P29 and P42. May I know which one should they follow?
Also, the package in P42 did have the D, E length information. Thank you.
…
Part Number: INA186 Hello Support team,
My customer try to investigate to improve noise performance on INA186. Do you have any application note? They tried Cf between IN+ and IN- and see any improvement. They would like to achieve more higher noise immunity…
Part Number: INA186 Other Parts Discussed in Thread: RCV420 I am looking to build a 4-20mA to 0-3.3V conversion circuit. The 4-20 mA input is generated by loop powered / externally powered (24V) process control transmitters (eg https://rishabh.co.in/uploads…
Part Number: INA186 Other Parts Discussed in Thread: INA185
Dear Technical Support Team,
Q1
My target spec is below. Current range is wide.
So I think shunt resistance should be low for maximum current.
Is it possible to use low VCM like 1mV?
For example…
Part Number: INA186-Q1 Other Parts Discussed in Thread: INA186 Dear team,
My customer wants to know what the max self-heating temperature of INA186A1QDCKRQ1 is. In my understanding, they want to know the max power consumption of our device. Could you please…