Part Number: INA195 Other Parts Discussed in Thread: OPA197 I'm having some issues with the INA195 in the following circuit configuration (there is also a 100nF decoupling capacitor for the INA195 not shown):
Initially, the circuit works as I would…
Other Parts Discussed in Thread: INA195 Hi,
I have a question.
If Vsense will be negative voltage, is the Vout 0V?
Normally the Vsense is positive, however the Vsense may becomes negative momentarily by the surge in our system.
It is no problem for our…
Other Parts Discussed in Thread: INA195 I need to measure high side current in a 80V nominal application. I will need 20V headroom above 80V to accommodate surge overvoltages, power supply tolerances etc. Maximum common mode in this application is 100V…
Other Parts Discussed in Thread: INA195 Hello,
I am using the INA195 current shunt monitor to measure the current draw of a 24VDC motor. I use a 30mOhm shunt resistor to measure typical motor currents of 1.2A. The supply voltage of the INA195 is +5V.
…
Other Parts Discussed in Thread: INA193A-EP Hi,
Can you clarify a couple of statements in the datasheet - http://www.ti.com/lit/ds/sbos307f/sbos307f.pdf
In the description on page 1 there is a statement saying that the part operates form -40 to -125C and…
Other Parts Discussed in Thread: INA195 , INA193 , INA194 Hello,
I have to sense current on 1ohm load, I found the INA195 from TI, it seem to be a good choice for this task but the problem is :
I want to measure small current en the load (something like…
Other Parts Discussed in Thread: INA195 Can you please clarify the issue of using the INA195/196 to measure current of -15V supply , even though the maximum absolute rating of the device is -16V ( stress issues ) .
If not how can I decrease the input cu…
Part Number: INA280 Other Parts Discussed in Thread: INA290 , TINA-TI , INA195 Is there already a pspice model for INA280 or a model that behaves similar.
Part Number: INA198 Other Parts Discussed in Thread: INA193 , INA196 , INA197 , INA194 , INA195 , Hi,
Full-Scale Input Voltage is specified 0.15V(typ).
How condition is this?
Best Regards,
Kuramochi