Part Number: INA237 Hi Experts
An customer is using INA237 as below.
Here are the registers dumped
0x00,0x0000
0x01,0xFB68
0x02,0x1000
0x03,0xFFFF
0x04,0x0000
0x05,0x0000
0x06,0x0CE0
0x07,0x0000
0x08,0x0000
0x09,0xFFFF
0x0A,0xFFFF
0x0B,0x0003
…
Part Number: INA237 Other Parts Discussed in Thread: TMP512 , INA209 Hi Team,
I would like to INA237 to replace EMC1702 on the customer board. However, EMC1702 has the #THERM pin, looks like INA237 didn't support this feature.
May I know is there…
Part Number: INA237 Hi team,
The datasheet shows the maximum value of rise time is 300ns. Is there any application risk when the rise time reaches 500ns under 100kHz frequency?
Best Regards
Silvia Gao
Part Number: INA237 Dear Team,
We plan to use INA237AIDGSR to detect two type adapters 48V and 54V,
Is there any risk for this design on INA237AIDGSR?
Many Thanks,
Jimmy
Part Number: INA237-Q1 Other Parts Discussed in Thread: INA237 Design Engineer has part# P INA237AQDGSRQ1 on the BOM, but I cannot find inventory. Could this part number be for Engineering Sample?
Part Number: INA237 Other Parts Discussed in Thread: INA327 , INA226 , Hi Team,
From the datasheet of VIL, can I understand the maximum 0.4V means the threshold that regard as low will not exceed 0.4V? For example, if the VIL = 0.5V, we cannot regard it…
Hi Jimmy,
I haven’t heard further update on this issue in a while. I’ll close the thread for now, please post back if you need assistance in the future.
Regards, Guang
Part Number: INA237 Other Parts Discussed in Thread: INA238 Hi team,
I found that INA237 and INA238 is hardware-p2p and they also had the same address selection and register map. My question is: if customer wants to replace IN237 with INA238, it's unnecessary…