Part Number: INA237 Other Parts Discussed in Thread: INA226 , hi senoirs,
I can't understand actual power power[W] reproduce from register POWER by these two coefficients 0.2*CURRENT_LSB, could you help clairy more detail about the POWER come from ?…
Part Number: INA237 Is it possible to extend measured bus voltage to 500VDC by using external resistor divider connected to VBUS? Current measurement is low side. Recalculation (including divider ratio) power and voltage is not a problem - is done externally…
Part Number: INA237 Team,
could you help on this?
At the moment we are experiencing Issues writing to the “CONFIG” register.
Values written to this register are obviously not stored. The strange thing is using the same write routine for…
Part Number: INA237 Hi,
I wanted to know the internal resistance value of INA237AIDGSR for calculating Rs value.For your reference attached a snapshot.
Thank you,
Vatsala Balol
Part Number: INA237-Q1 Hi,
I am using the INA237-Q1 to monitor the voltage,current and power.
After writing the value(0x2003)/0x9001 to the Shut calibration register.
For Input voltage is 50V, Current register updated with the value which corresponds…
Part Number: INA237 Other Parts Discussed in Thread: SYSCONFIG Hello everyone,
My customer wants to design the INA237 in their system.
But currently they have voltage; current and power register value issues.
They need to know the actual value based…
Part Number: RM46L852 Other Parts Discussed in Thread: INA237 , , SYSCONFIG Dear Champs,
My customer connected INA237 to RM46L852 through I2C, but failed to communicate with INA237.
As there is no implementation for I2C communication in below sysconfig…
Part Number: INA237 Hi team,
I have connected eight (INA237)devices in a single bus. I doubt it will affect the racing time.
What are the Pin Capacitance (SDA, SCL) and the total capacitance of one bus line Cb?
Thanks, Regards
Anoop Varma m
Part Number: INA237 Hi,
in our project, INA237 used to monitor 28V voltage, current and temperature; after board power up, register 3eH can be read, but temperature, current and voltage are always 0H,
below value get from InA237:
sudo i2cget -y 1 0x40…
Part Number: INA237 Other Parts Discussed in Thread: SYSCONFIG Hi
I was trying program INA237 with MSP430F229. Is there any predefined libraries that was provided by TI for all the initial configuration of register in INA237. If so where i could find…