Part Number: INA260 Hi Team, is it possible to measure a pulsed current with INA260. If the sample time is long enough. The datasheet mentions that the longest sampling time is 8.244 ms. If the signal is at least 10 times faster, would it give a good average…
Part Number: INA260 Hello,
I need to measure stray voltage on pins of PCB board. If stray voltage is present within the threshold, then current will be sent out of the same pin. I also need to measure this current as well.
For this application I am planning…
Part Number: INA260INA260 have two fetures to average and make the signal better the time to take the sample and the oversampling of the signal. How to combine this to the software.
I have a signal that is from a motor and this signal is quite jumping…
Part Number: INA260 Other Parts Discussed in Thread: INA240 , INA253 Hi team,
My customer is using the INA260AIPW to measure the current (1.4Amax) for one phase of a 5-phase pulse motor. The motor voltage is 24V. The INA260 is placed between the push-pull…
Part Number: INA260 Hi,
Could you please let us know the MAX of package resistance value? On the datasheet, Typ of package resistance is 4.5mm_ohm. But my customer wants the MAX value. Please advise us.
Thanks and best regards, M.HATTORI.
Part Number: INA260 Hello,
I have a problem with measuring negative currents. The INA260 works fine and I can read the I2C address. But if I switch the -15.7V to this, the INA260 is destroyed and the VCC-X goes back to 3.2V. What am I doing wrong?
With…
Part Number: INA260 Other Parts Discussed in Thread: INA169 , INA219 , , INA228 , INA229 HI team, Good day. Our customer has INA260 breakout board from Adafruit and they measure the current and power consumption of a motor that draws 5A. The current printed…
Part Number: INA260 We actually used two ina260 chips, one on the 12V pass and one on the 5V pass. Both chips use the same IIC set
But when both paths are empty, The current value read by 5V port is 16381 The current value read by 12V port is 0
Although…
Part Number: INA169 Other Parts Discussed in Thread: INA260 , , INA190 , INA229-Q1 , INA228-Q1 Hello Guys,
Good day.
Our customer is using INA260 in measuring the current, voltage and power using Adafruit on the link below using their sample code ina260_simpletest…