Vidhya,
If this is the case, the scope shot demonstrates that the load current is the issue. Whether or not the INA282 is doing something impedance-wise at the inputs to distort the load line is up for debate, but the scope shots clearly show the same…
Hello Dharma,
Since it has been over a month from your question, I will go ahead and close out this post and mark as resolved.
If issue is not resolved or you still have other questions, please post back to the forum.
Sincerely,
Peter
Part Number: INA282 Other Parts Discussed in Thread: INA240 , Hi Current Sensing Folks,
Does TI have p2p device for INA282AIDR? Otherwise, could you help suggest any similar device even though it's not p2p? Thank you.
Part Number: INA282-Q1 Other Parts Discussed in Thread: ADS1118 Hello,
We are using external ADC (ADS1118IDGSR) . for current sensing by IC INA282-Q1. We have connected shunt resister of value 0.0001ohm(connected 0.0003ohm in parallel manner) at high side…
Part Number: INA282 Other Parts Discussed in Thread: INA210 , INA302 , INA240 , INA190 Hello,
I am Using current INA282 Current sensor (Bi-Direction).
My Current range is from 100mA to 13.5A in one direction and in another direction the Current range is 100mA…
Part Number: INA282 Other Parts Discussed in Thread: INA201 , INA193 , INA226 , INA220 Hi team,
I have questions on BW of current sensor.
1. INA282 has 10kHz of BW, which is quite narrow when it's compared to other INA parts such as INA193 and INA201 (300kHz…
Part Number: INA282 Other Parts Discussed in Thread: LM7705 Below is the circuit I'm trying to test. Without a load I'm measuring 8mV at the output. I've built 6 copies of this circuit and all behave the same. In 2 instances I measured 0V at the output…
Part Number: INA282 Other Parts Discussed in Thread: INA283 Hello, I am using the INA282 in a new design. I inserted a schematic showing how I am using this part in the design. The bus supply is 15.7 VDC. The nominal power draw to the "Trillium_Power…
Part Number: INA282 Hi! I want to measure alternating currents from 5mA to 1A from 220VAC and thought of INA282. I want to use it on low side as in the schematic below, is it possible?
The circuit will be "open" until the triac receives signal, then it…
Part Number: INA282 Hi,
customer use INA282 with VSSOP package in high precision battery test equipment,and have a problem about the output voltage. the schematic as below, current sense resistor is 0.01ohm.
During the battery charge and discharge, current…