Part Number: INA293 I need to measure the current of a signal with at least 1 nanosecond precision. The signal is a 400kHz square wave with under 20% duty. This signal will have a peak voltage of 50V and a peak current of 4.5A. Is the INA293 good enough…
Part Number: INA293 Other Parts Discussed in Thread: OPA188 , BUF634A , THS3491 Hi Team,
I want to design an electronic dc load. I drew a test board as in attachment. I have some concerns and questions about the design in schematic.
1. I plan to use INA293…
Part Number: INA293-Q1 We have a simple current sense circuit and we measure the current from a 2 mOhm sense resistor from a high side of 28 Vdc.
Current to be measured is inductor current which has a switching frequency of 300 kHz.
Below CH2: Voltage…
Part Number: INA293-Q1 Other Parts Discussed in Thread: INA293 Hello, I am using INA293A4QDBVRQ1 in a design. I placed the current sense circuit near the power input so I can measure the current of the whole board. When I measured the current, I got very…
Part Number: INA293 Hallo together ,
we are planning a design with the INA293B1, where we want to measure a shunt current and want to detect a short-circuit current.
To detect the short-circuit current as fast as possible we need the full slew rate of…
Part Number: INA293 Dear Sir or Madam,
Please could you inform me about Moisture Sensitivity Level (MSL) of the part INA293A2QDBVRQ1.
Thanks in advance.
Best Regards,
Kaoutar Ben Kaddour
eDFM Engineer at SLB
KKaddour3@slb.com
+447576895512
Hello Carolus, Kai and Clemens,
Thank you very much for your replies and I 'm sorry to be late my response. These replies are very helpful for the customer. The customer understood INA293 output structure and capability because of you.
Thank you again…
Part Number: INA293 Dear Sir or Madam,
I am writing to know Moisture Sensitivity Level (MSL) of INA293A2QDBVRQ1.
Thanks in advance.
Best Regards,
Kaoutar Ben Kaddour
Part Number: INA293 Dear Sir or Madam,
I am writing to know the terminal finish of INA293A2QDBVRQ1 if it is NiPdAu or NiAu or Au. Please could you tell me the thickness of Au.
Thanks in advance.
Best Regards,
Kaoutar Ben Kaddour