Part Number: INA293-Q1 Other Parts Discussed in Thread: INA293 Tool/software: What is the recommended approach to adding a common-mode filter to the input of an INA293?
Datasheet section 8.1.2 addresses differential mode filtering, but not common-mode…
Part Number: INA293-Q1 Other Parts Discussed in Thread: INA293 , INA281-Q1 , , INA310A Tool/software: Hi,
Currently, we need to achieve current sensing data with a bandwidth of over 2 MHz on the platform.
We have surveyed the TI INA293, which can provide…
Part Number: INA293-Q1 We have a simple current sense circuit and we measure the current from a 2 mOhm sense resistor from a high side of 28 Vdc.
Current to be measured is inductor current which has a switching frequency of 300 kHz.
Below CH2: Voltage…
Part Number: INA293-Q1 Other Parts Discussed in Thread: INA293 Hello, I am using INA293A4QDBVRQ1 in a design. I placed the current sense circuit near the power input so I can measure the current of the whole board. When I measured the current, I got very…
Part Number: INA293-Q1 Other Parts Discussed in Thread: INA293 Hello! I am using the following current sense opamp from TI: INA293A3 connected on this way:
The device is working very nice from when the output of this devide is on the range from 700mV…
Part Number: INA293-Q1 Other Parts Discussed in Thread: INA293 Hi,
We are using INA293-Q1 and want to add output low pass filter going into our ADC. I am targeting 100ohm and 10nF.
Is the output stable for this condition? How do I choose the output RC…
Part Number: INA293-Q1 Other Parts Discussed in Thread: INA240 , INA293 , DRV8323 , INA241B , INA180 , INA281
Hi
Is it possible to measure the phase currents of a three phase motor control application with the INA293-Q1? I used the INA240 before and this…
Part Number: INA290-Q1 Other Parts Discussed in Thread: INA293-Q1 , , INA293 , INA290 Hi TI,
We like the improved quiescent current of INA290-Q1 with only slightly less nominal bandwidth. Is INA290-Q1 recommended for our automotive 48V DC-DC converter application…
Part Number: INA310B-Q1 Other Parts Discussed in Thread: INA293 Tool/software: I would like to set up input filter on the INA310B1QDGKRQ1, what is the gain error factor for this?