Part Number: INA300-Q1 Hi team
INA300-Q1 D/S say Input bias current = Max 0.5uA for disable mode.
so total input bias current would be Max 1uA(= 0.5uA x 2) for two input pins ?
further, I have to double the graphed Ib on Figure 8(Disabled) for two input…
Hello Javier,
The issue of INA300-Q1 is solved, now the alert signal goes low when i applied 2A load.
I have added RC filter circuit of capacitor 100nF and Resistor 22ohm value.
But now the new problem is arises that when i have added switch & control…
hello Simmons,
I am talking about MOSFET Q2, which was heated very fast, when we will pass 2A current in this circuit.
I have attached INA300-Q1 schematic herewith, in that i made some changes like, i want to keep this circuit in transparent mode so…
Part Number: INA300-Q1 Hi Sir
INA300-Q1 is for Over Current Protection.
We would like to implement the similar function but low current detection
Load current of 5mA flow through RSENSE = 10mohm
The differential voltage = 50uV
Does INA300-Q1 is…
Part Number: INA300-Q1 Other Parts Discussed in Thread: INA300 I'm currently using the INA300 chip in conjunction with a 0.0003 Ohm current sense resistor to ultimately set an overcurrent limit of 90A. However, in testing the chip prior to inserting into…
Part Number: INA300 Other Parts Discussed in Thread: INA200-Q1 , INA200 , , INA293 , TLV3201 Dear Team,
Due to PD 3.1 will support EPR (up to 48V voltage), my customer requires a solution to replace previous INA300A.
Could you help to recommend a similar…
Part Number: TPS1HB08-Q1 Other Parts Discussed in Thread: INA300-Q1 , INA300 , , TPS25940-Q1 , TPS1H100-Q1 This question regards multiple products in the TPS1H*, TPS1HB*, and TPS2HB* families.
Context: I am considering use of the TPS1HB08-Q1 in an application…
Part Number: INA301-Q1 Other Parts Discussed in Thread: INA301 , INA300-Q1 , INA200 , INA200-Q1 , INA193 , INA191 , INA186-Q1 , INA190-Q1 , , INA300 How do I estimate the input bias current for a lower supply for example 3.3V? And how do I estimate the max bias…
Part Number: INA200 Other Parts Discussed in Thread: INA240 , INA381 , INA293 , INA303 , INA302 , INA301 , INA300 , INA290-Q1 Hi,
When using INA200 for short circuit current sensing,the output of amplifier(Vbus) is wrong.
As shown below,there are two possible…
Other Parts Discussed in Thread: INA225-Q1 , INA300 , INA225 , TIDA-00328 Hi
I'm considering the current sense system very wide range.
The range is about 100A from 0A.
So, I'm looking for a current shunt monitor can also be output at low input.
…