Part Number: INA302-Q1 Hi,
We are using INA302A3QPWRQ1 in the design. Please provide response for the below queries
1)How the offset voltage varies with temperature? Whether offset voltage increases with temperature or vice versa? The value provided is…
Part Number: INA302-Q1 Other Parts Discussed in Thread: INA302 Hi team,
I plan to use this device to monitor VBAT current of automotive ECU.
In order to minimize system standby current, I plan to stop supplying VS to INA302-Q1 in Standby condition.
…
Part Number: INA302-Q1 Hi sir,
Could you let me know what is INA302-Q1 supply current consumption? My customer want to check their power design.
Thanks.
Part Number: INA302-Q1 Other Parts Discussed in Thread: INA302 , INA303 Hi Team,
I am planning to use INA302 for current sensing and overcurrent protection. Since INA302 is a bidirectional device where the reference pin can be offset with a particular voltage…
Part Number: INA302 Other Parts Discussed in Thread: INA303 Hi team,
Could you help review the INA302A2 schematic and provide your comments? Thanks!
Common mode voltage= 24V
Alert trip point= 20A with 1ms delay
Best regards,
Sam Ting
Part Number: INA302 I want to use INA302 for my current sense application, my question is can i use this device in low side current sensing application..Because i only find references in which it is used in high side.
Thank you
Part Number: INA302 I am using your P-Spice model to simulate the operation of the INA302A1. Model only works partially.
Limit 1 and Limit 2 pins work correctly with 80uA of current:
LIMIIT1 = 1K50 = 120mV = 60mA with 100mOhm Isense resistor.
LIMIT2 …
Other Parts Discussed in Thread: LP87563-Q1 , LM5143-Q1 , LM25141-Q1 , LM51561-Q1 , LM7480-Q1 , INA302-Q1 hi, Sir
Can your provide each parts excel design tool for LM7480-Q1, INA302-Q1, LM25141-Q1, LM51561-Q1, LM5143-Q1, LP87563-Q1 ?
Part Number: INA302-Q1 Other Parts Discussed in Thread: TINA-TI
Hi team,
I simulated the start up behavior using TINA-TI model on TI.com and found that there is about 150us start up delay
only when I connect REF to GND(this is my use case).
If I apply…
Part Number: INA302 Team,
A customer would like to monitor current and would like to have different curent levels for which an alert should be generated. To achieve this, the idea would be to use two INA302 in parallel.
Is there anything that needs to…