Part Number: INA592 Hi Team, Our customer would like to confirm if is it ok to use such a low-valued load to INA592? He would like to confirm if it is better than AD8276 (please see figure 20 and fig. 21) where they show the max. output voltage as a function…
Part Number: INA592 Hello, See: www.ti.com/.../ina592.pdf In my opinion, figure 79 contains an error. The voltage at the output is: (V+) x 0,33 because of 12k and 6k resistor divider. Best Regards Axel Kretzschmann DESY Zeuthen Platanenallee 6 15738 Zeuthen…
Part Number: INA592 Hi,
I have a question about the offset voltage specification.
Vos is up +/-40uV when G=1/2 (or +/-80uV when G=2). From the datasheet, the upper part of the table is titled "OFFSET VOLTAGE (RTO)" but the specification in table says…
Part Number: INA592 Hello
I am planning to design a resolver interface based on this application note
https://www.ti.com/lit/an/slyt776/slyt776.pdf?ts=1647466850245
I noticed on page 2 , figure 2 that the voltage buffers are in positive feedback…
Part Number: INA592 Hi Team,
Good day.
Customer is asking if we have a pspice of INA592 that has a gain of 2. According to them, the PSPICE found in the website has only 1/2 gain. Can you please confirm?
Thank you and looking forward for your kind…
Part Number: INA592 I am operating INA592 with Gain 2 configuration adn with a Single Supply of 2.5V.
I am using it to correct the offset and hence the signal is given to REF and the TI DAC 7571 output is given to Sense. With both the inputs at 2.5V…
Part Number: INA592 Other Parts Discussed in Thread: INA818 Hi expert,
From below figure, the max common mode input high of INA592 is 54V:
However, from datasheet, the max input voltage is 3V+.
So I'm a little confused, if I use single supply…
Part Number: INA592 Other Parts Discussed in Thread: INA149 Hello Guys,
Good day.
Our customer is using this component (INA592IDGKR) to record cell voltage data from a stacked battery system. The one drawback this has is they also need to stack the…
Hi Martin,
Q: c) The INA592 offers the package variant DRC (VSON-10) but is currently labelled as "Preview". Is there a roadmap when this package is available?
I was told that we are looking to RTM by the end of this month (barring any setbacks).…