Part Number: ISO1042 Hello,
We need an isolated CAN transceiver which also features 'hot-plug'. But I cannot find one within the isolated CAN transceiver category.
After some research into the existing the product which marked as 'hot-plug capable…
Part Number: ISO1042 Customer is now using ISO1042 in industrial application. they'd like to know if the ESD capability is related to its input impedance on every pin of the device?
For example, The higher input impedance, the higher ESD immunity…
Part Number: ISO1042-Q1 Other Parts Discussed in Thread: ISO1042 , ABS Hi,
My customer is having the following glitch on the power up and this is throwing other nodes on the bus into trouble:
This is happening on power up of the inverter (around 30ms from…
Part Number: ISO1042-Q1 Other Parts Discussed in Thread: ISO1042 Hi
We are currently facing a technical challenge right now as we use :
- 2 Batteries 12 V in series and 2 DCDC (each DCDC connected to a battery 12V)
- DCDC1 is connected to a 12V batteries…
Part Number: ISO1042 Hi Team,
My customer is using ISO1042, and they are asking about the minimum and maximum spec of tR and tF(differential output signal rise/fall time), do we have data for it?
Thanks.
Part Number: ISO1042-Q1 Other Parts Discussed in Thread: ISO1042 , TEST Hi Experts,
My customer wants to drop in replacement from TJA1052IT/5 to ISO1042. Cross reference tool says it can be drop-in replacement. There are two different pin. These pins of…
Part Number: ISO1042 Hi there!
I want to have a pin compatible situation with the IL 41050TE. This device has a Vref output at pin 10.
Is it possible to let PIN 10 of ISO1042 floating? or do i have to connect it to GND2 with a 0ohm resistor?
Part Number: ISO1042-Q1 Hi,
For the 16 pin layout of ISO1042-Q, there are several not connected pins.
Is it possible to use NC pins connected to ground (low or high)? What are the consequences?
Thanks in Advance
Emre
Part Number: ISO1042 When trying to transmit at 5 Mbps we see the device transition to the higher speed, but quickly stop transmitting (just right of center on scope shot). In attached scope shot Purple is CANH blue CANL and Red is a math function "CANH…
Part Number: ISO1042-Q1 i am using ISO1042DWVR and desinging the power supplies of the IC. what is the rated or maximum current need by the IC ? Vcc1 is 3.3 volt and Vcc2 is 5V. how much should be the power level of the 3.3v and 5v supply rail ?