Part Number: ISO1042 I am looking for an IC or a design solution that will convert USB to CAN with 4kV insulation and 8kV creepage. ISO1042 looks OK, but it is not USB.
Part Number: ISO1042-Q1 Other Parts Discussed in Thread: ISO1042 Hi there,
I have recently design an isolation CAN connecion, looks sample while I have one confusion about following 2 article:
Figure 1 of: http://www.ti.com/lit/an/slla298d/slla298d.pdf…
Part Number: ISO1042 Hi,
The schematic is:
CANH-CANL waveform is: there is a small jump in the red circle.
What may cause it and how can we solve the problem?
StefanG,
There are only a couple more things I can think to do here.
Lowering data rate could help and might be the simplest approach.
The other suggestion is using a CAN transceiver with lower Differential input capacitance C(ID). This is essentially…
Part Number: ISO1042-Q1 Other Parts Discussed in Thread: ISO1042 , SN6501 Hi,
I have designed isolated CAN using ISO6501, ISO1042 and Pulse transformer.
For space saving and better track routing I have put transformer on one side of the PCB and ISO1042…
Part Number: ISO1042-Q1 Other Parts Discussed in Thread: TEST In the related thread Lucas_Schulte9 posted, that he has some additional informations on the ISO 11898-2:2016 test standard for the ISO1042-Q1 which cannot be shared on the forum.
I would also…
Part Number: ISO1042 Other Parts Discussed in Thread: TEST Hi Team,
My customer reported an issue while using ISO1042: the CANH/CANL signal oscillated while connected to CAN BUS.
Could you kindly help give comments on below 2 items:
Comments on…