Part Number: ISO1042-Q1 Other Parts Discussed in Thread: ISO1042 Hi
We are currently facing a technical challenge right now as we use :
- 2 Batteries 12 V in series and 2 DCDC (each DCDC connected to a battery 12V)
- DCDC1 is connected to a 12V batteries…
Part Number: ISO1042-Q1 Other Parts Discussed in Thread: ISO1042 Hi Experts,
My customer wants to drop in replacement from TJA1052IT/5 to ISO1042. Cross reference tool says it can be drop-in replacement. There are two different pin. These pins of ISO1042…
Part Number: ISO1042-Q1 Hi,
For the 16 pin layout of ISO1042-Q, there are several not connected pins.
Is it possible to use NC pins connected to ground (low or high)? What are the consequences?
Thanks in Advance
Emre
Part Number: ISO1042-Q1 Dear TI..
I'm using ISO1042-Q1.
By the way, the following waveform(Fig.#1) is checked.
Why did the last waveform level come out high?
(The micro-controller is using STM8AF5286.)
Still, I would like to know the detailed reason…
Part Number: ISO1042 Hi there!
I want to have a pin compatible situation with the IL 41050TE. This device has a Vref output at pin 10.
Is it possible to let PIN 10 of ISO1042 floating? or do i have to connect it to GND2 with a 0ohm resistor?
Part Number: ISO1042 When trying to transmit at 5 Mbps we see the device transition to the higher speed, but quickly stop transmitting (just right of center on scope shot). In attached scope shot Purple is CANH blue CANL and Red is a math function "CANH…
Part Number: ISO1042 Hi Team,
My customer use this part now , but his loop2 T prop is 690ns and his RL is 150ohm / CL is 2.2nF.
And I suggest them to change to RL : 60ohm and CL : 100pF will run in right way. Right ?
But they still wonder to know how…
Part Number: ISO1042 Hi,
Could you please let me know about ICC2 consumption. Datasheet show as below:
- TXD = 0 V, bus dominant, RL = 60 Ω: 73.4 mA(MAX) - TXD= VCC1, bus recessive, RL = 60 Ω: 4.1 mA(MAX)
In common use case, some nodes connect…
Part Number: ISO1042-Q1 i am using ISO1042DWVR and desinging the power supplies of the IC. what is the rated or maximum current need by the IC ? Vcc1 is 3.3 volt and Vcc2 is 5V. how much should be the power level of the 3.3v and 5v supply rail ?