Part Number: ISO1176 Dear Technical Support Team,
・ About ICC2 described in the ISO1176 datasheet (7.6 Supply Current)
> ICC2 5.25V DE at VCC1, 25 Mbps, 54-Ω load: 75mA
This value is ・ Current consumption on the 5V logic side of ISO1176 ・ 5V terminating…
Part Number: ISO1176 Other Parts Discussed in Thread: ISO1450 Hi everyone ,
Could you please tell me how can I connect the pins of ISODE and PV ? Can I use pull up /down resistor?
Part Number: ISO1176 Other Parts Discussed in Thread: PROFIBUS , , ISO1450 , ISO1430 Section 10.2.2.2 of the datasheet details what is called a 'Sticky Bit' issue of this chip. However, I'm struggling to tell if this applies in our application as I'm…
Part Number: ISO1176 Other Parts Discussed in Thread: PROFIBUS , ISO1452 , ISO1432 Hi team
Here customer use ISO1176 in their products, and had below queries need your help:
1.how to select the common mode inductor for differential output and bypass…
Part Number: ISO1176 Hi Team
When using ISO1176, if A B pin connected with DP interface wrong inversely, what kind of the influence would have?
currently it is inversely connected, but communicate normally. While correct the connection, failed to…
Part Number: ISO1176 Other Parts Discussed in Thread: PROFIBUS Dear Technical Support Team,
How does ISO1176 keep DC level output when input DC level ?
If it doesn't how does it change on output?
Best Regards,
ttd
Part Number: ISO1176
Dear Technical Support Team,
Could you share the failure mode(open or short or drift) of ISO1176DW?
There are some shorted case between vcc and output.
■Case1
Shorted between Vcc1 and R
■Case2
Shorted between Vcc2…
Part Number: ISO1176 Hi, Could you tell me about ISO1176 worst case current consumption? 1.Vcc=5V , Terminating resistor = 50ohm, sampling rate =20Mbps Customer wants to know the maximum current consumption for the above condition. 2.Could you check…
Part Number: ISO1176 In the datasheet of ISO1176, there are two kinds of solder pad recommended as showed below. In which circumstances are they used? Which one should I choose? My isolation voltage is 1.5 kV.