Part Number: ISO120 Hello,
I would like to know the applicable standard (for testing: AEC-Q101, JEDEC...) for the ISO120SG. Do you have ny reliability data to share? For example, life test, Thermal cycles, 85°C/85RH, HAST, and any other?
Do you also…
Part Number: ISO120
URGENT
Hello,
I am planning on using the ISO120SG (with C1=C2=0) in an application where there will be 6kV/us IMV transients that are 0.020 us long (and that occur at a fixed 40 kHz frequency/every 12.5 us).
The ISO output will…
Other Parts Discussed in Thread: ISO120 Hi team,
One of our customer is using the ISO120 in their system for sensor isolation. Wanted to know if it has a cold sparing feature, i.e. is it OK to have the signal on the Com pin before the device is powered…
Other Parts Discussed in Thread: ISO120 Hi,
The ISO120 has an application note to boost the BW of the device to 100kHz (which is what I need). I plan to use the ISO amp to separate an amplified signal from an amplifier stage (between 1-5V) and the oscilloscope…
I want to control the generation of high voltages i.e; around 5000V in dc/dc converters using transformer by controlling the duty cycle of switch in primary circuit through PWM regulator.As high voltage PWM IC's are not avaliable can i use above mentioned…
Part Number: ISO121 Other Parts Discussed in Thread: ISO224 , ISO120 , PSPICE for TI comes with ISO121X Model and when using it to simulate a simple application circuit, it results in several netlisting errors as shown below and simulation does not run,…
Part Number: ISO124 Other Parts Discussed in Thread: ISO122 , ISO224 , ISO120 , Greetings!
My problem is: i need to do a simulation, using the Eagle Software, but i don't have the PSPICE model for ISO124U.
I made a research and found anothers components…
Part Number: ISO124 Other Parts Discussed in Thread: ISO120 , ISO224 , ISO121 Hi TI Support,
I am using ISO124 in our current project, I would like to run PSPICE simulation but there was no model for it. I saw ISO120 has a model, perhaps I can use it as…