Part Number: ISO1211 Tool/software: Dear sir or madam
In an STO application (safe torque off) we implemented two ISO1211 for the input signals. As the maximum length of the STO input cables are limitted to < 30m withstanding of surge tests is not required…
Part Number: ISO1211 Other Parts Discussed in Thread: TIDA-01599 , ISO1228 Tool/software: Good day, collogues,
My customer would like to use the ISO1211 for an STO circuit. They have reviewed the documents “Overview STO Concept TIDA-01599” and the associated…
Part Number: ISO1211
Tool/software:
Hello,
I'm currently debugging the design of a peer and I was wondering if this is a normal use case:
As one can see there are plenty of differences between this design and the reference design ( https://www…
Part Number: ISO1211 Hello ! We needed help with a product design/suggestion for a circuit. I am Avaneesh ketan and I am working on Remotely Operated Vehicles (ROV)/Robots for Underwater applications. Our problem description
We control the ROVs using Joysticks…
Part Number: ISO1211 This electronic desing would be robust enough to withstand a very noisy 120 Vac line, with a 400/120 VAC three-phase transformer as its source. Connected in parallel on this 120 Vac line are the coils from the electric coupling contactors…
Part Number: ISO1211 Hello Team,
What would output from ISO1211, if RTHR is shorted and lead to a large input current and eventual device damage? (High/ Low/ Hi-Z)
We are thinking of using ISO1211 to input DC110V.
Regards,
Taiki Koga
Hi Koteshwar Rao ,
Thank you for your kind support,
Actually,We use ISO1211 for AC 220V detect function in our product design ,
and we refer circuit as below :
Q1 : If we want the ISO1211 output is stable DC voltage level , could I adjust Cin cap value ? …
Part Number: ISO1211 Other Parts Discussed in Thread: TINA-TI , TVS3300 Hello.
I am simulating a digital input model with TINA Tool, with de IC ISO1211, I can't found the ISO1211 model, there is a ISO121x Model, but the pins are very diferent from the…