Part Number: ISO1211 Hi. We are making a digital input board using ISO1211 IC of TI. We work on high tension lines and 132Kva transformers. Our clients are Indian railways and electric distribution company. We face high transient voltage and surge. I…
Part Number: ISO1211 Hi,
I am looking for a solution where iso1211 should be used in wet and dry contact using simple DIP switch is there any solution for the following.
For example
1.If we use input1 in WET contact that can be changed using simple DIP…
Part Number: ISO1211 Hi,
My customer has two questions regarding ISO1211.
Firstly, they want to utilize ISO1211 to do ac voltage detection. They want to know more details about the detection mechanism, when ISO1211 senses the ac voltage, does it sense…
Part Number: ISO1211 Hello team.
One customer considers to use our ISO1211 device in digital input modules for Programmable Logic Controller.
As customer claims, test for IEC 61000-4-6 compliance is mandatory for such kind of end application.
On ti.com…
Part Number: ISO1211
Hi,
I want to use ISO1211 for threshold detection of 0v-24v. However the field side 0-24V is noisy environment.
Datasheet says ISO1211 have capacitive coupling. I wonder if the field side noise can came to output pin of iso 1211…
Part Number: ISO1211 Hi Team,
Our customer would like to use ISO1211 to translate a digital signal from 12V into a 5V (TTL) signal. The datasheet shows that INx and SENSEx pins can accept voltage from –60V to 60V. However, the datasheet also shows that the…
Part Number: ISO1211 Other Parts Discussed in Thread: TPS62095 Tool/software: Code Composer Studio Where can I get iso1211, tps62095 belongs to LT spice model or PSpice model (unencrypted) files
Part Number: ISO1212 Other Parts Discussed in Thread: ISO1211 Hi team,
What is the difference between ISO1212 and ISO1211 when applied to AC input? which one is better?
Could you share ISO1212 reference schematic when applied to AC input. thanks
Part Number: ISO1211 Hello team,
As we could ignore IEC61131-2, how much can we reduce the current limit for ISO1211 in order to minimize the self-heating of ISO1211?
While, does the lower current limit cause the lower noise immunity (or slower propagation…