Part Number: ISO1410DWEVM
Hi,
In our circuit design, the ISO1410DW device is used along with supporting internal circuitry on a single board. Multiple identical boards are connected in parallel on a common RS-485 bus. The RS-485 network is interfaced…
Part Number: ISO1410DWEVM Other Parts Discussed in Thread: ISO1450 , ISO1410 Dear Team, Can the ISO1410DWEVM be used for the evaluation of the ISO1450DWR as well ? Regards, Nir
Part Number: ISO1410DWEVM Other Parts Discussed in Thread: ISO1410 I am using this part in an environment where the DC common mode floating voltage incident on the chip inputs can go up to 1500V. There can be about 200 units connected on the RS485 bus…
Part Number: ISO1410DWEVM Other Parts Discussed in Thread: SN65HVD11-HT I need a high temperature package with robustness similar to ISO1410DW. Tolerance to sustained temperatures above 250C will be necessary. Does this exist?
Hello Anatol,
Unfortunately, we do not have these boards available for purchase for this design. However files are provided here: https://www.ti.com/tool/TIDA-00333
Separately if you are trying to evaluate the device, you might also consider the following…
Hello Meghana,
The ISO1410DWEVM Evaluation board will be the best reference for a typical layout for the ISO1430. Please let me know if you have specific questions!
Best, Andrew
Part Number: ISO3082 Other Parts Discussed in Thread: ISO485EVM , ISO1410DWEVM , ISO1410
Hi,
I am using ISO3082DWG4 for my RS485 circuit. In that, We define chip characteristics in .dts file as per below.
After that, when we establish connection…
Hi Jim,
Thanks for your inputs. We a few isolated RS-485 devices that can also be used for RS-422. Most of these devices are available in a single full-duplex / half duplex transceiver options. Please do have a look at the below device and its associated…